<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX RTOS link application to SDRAM in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTOS-link-application-to-SDRAM/m-p/1829425#M18831</link>
    <description>&lt;P&gt;Can someone please give a document on how to link MQX RTOS application to SDRAM?&lt;/P&gt;&lt;P&gt;We tried the below mentioned procedure. It works for bare metal projects but not for MQX example projects.&lt;/P&gt;&lt;P&gt;Image running from external SDRAM&lt;BR /&gt;• MCUXpresso IDE&lt;BR /&gt;1. Select Project &amp;gt; Properties - C/C++ Build &amp;gt; Settings &amp;gt; Tool Settings &amp;gt; MCU Linker &amp;gt; Managed&lt;BR /&gt;Linker Script and check Link application to RAM.&lt;BR /&gt;2. Select Project &amp;gt; Properties - C/C++ Build &amp;gt; Settings &amp;gt; Tool Settings &amp;gt; MCU C Compiler &amp;gt;&lt;BR /&gt;Preprocessor and add defined symbol SKIP_SYSCLK_INIT=1.&lt;BR /&gt;3. In Project &amp;gt; Properties &amp;gt; C/C++ Build &amp;gt; MCU settings, delete Flash, and modify BOARD_SDRAM to&lt;BR /&gt;start at 0x80002000 with size 0x1dfe000. Move BOARD_SDRAM to first position to make it default.&lt;BR /&gt;4. Build the image.&lt;/P&gt;</description>
    <pubDate>Fri, 15 Mar 2024 13:10:26 GMT</pubDate>
    <dc:creator>Vidya_1203</dc:creator>
    <dc:date>2024-03-15T13:10:26Z</dc:date>
    <item>
      <title>MQX RTOS link application to SDRAM</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTOS-link-application-to-SDRAM/m-p/1829425#M18831</link>
      <description>&lt;P&gt;Can someone please give a document on how to link MQX RTOS application to SDRAM?&lt;/P&gt;&lt;P&gt;We tried the below mentioned procedure. It works for bare metal projects but not for MQX example projects.&lt;/P&gt;&lt;P&gt;Image running from external SDRAM&lt;BR /&gt;• MCUXpresso IDE&lt;BR /&gt;1. Select Project &amp;gt; Properties - C/C++ Build &amp;gt; Settings &amp;gt; Tool Settings &amp;gt; MCU Linker &amp;gt; Managed&lt;BR /&gt;Linker Script and check Link application to RAM.&lt;BR /&gt;2. Select Project &amp;gt; Properties - C/C++ Build &amp;gt; Settings &amp;gt; Tool Settings &amp;gt; MCU C Compiler &amp;gt;&lt;BR /&gt;Preprocessor and add defined symbol SKIP_SYSCLK_INIT=1.&lt;BR /&gt;3. In Project &amp;gt; Properties &amp;gt; C/C++ Build &amp;gt; MCU settings, delete Flash, and modify BOARD_SDRAM to&lt;BR /&gt;start at 0x80002000 with size 0x1dfe000. Move BOARD_SDRAM to first position to make it default.&lt;BR /&gt;4. Build the image.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 13:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTOS-link-application-to-SDRAM/m-p/1829425#M18831</guid>
      <dc:creator>Vidya_1203</dc:creator>
      <dc:date>2024-03-15T13:10:26Z</dc:date>
    </item>
    <item>
      <title>Re: MQX RTOS link application to SDRAM</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTOS-link-application-to-SDRAM/m-p/1835070#M18838</link>
      <description>&lt;P&gt;Hi Vidya:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would suggest you can check below link, it is about SDRAM configuration with FreeRTOS.&amp;nbsp; It maybe similar to MQX&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/SDRAM-configuration-on-MIMXRT1050-EVK-B-using-FreeRTOS/m-p/878903/highlight/true" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-IDE/SDRAM-configuration-on-MIMXRT1050-EVK-B-using-FreeRTOS/m-p/878903/highlight/true&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Another demo you can refer to is Kinetis K70,&amp;nbsp; there is a DDR build configuration in classic MQX 4.2&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 26 Mar 2024 04:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTOS-link-application-to-SDRAM/m-p/1835070#M18838</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2024-03-26T04:22:17Z</dc:date>
    </item>
  </channel>
</rss>