<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic YOcto flash emmc fails in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/YOcto-flash-emmc-fails/m-p/1783972#M18821</link>
    <description>&lt;P&gt;I am building image as such:&lt;/P&gt;&lt;P&gt;export MACHINE=imx8mqevk&lt;BR /&gt;DISTRO=fsl-imx-wayland MACHINE=${MACHINE} source imx-setup-release.sh&lt;/P&gt;&lt;P&gt;andflash using :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;sudo ./uuu -b emmc_all imx-boot-imx8mqevk-sd.bin-flash_evk core-image-base-imx8mqevk.wic.bz2&lt;/P&gt;&lt;P&gt;device do not print anything on boot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;to test I flashed the demo image:&amp;nbsp;&lt;/P&gt;&lt;P&gt;sudo ./uuu -b emmc_all imx-image-full-imx8mpevk.wic&lt;BR /&gt;&lt;BR /&gt;which works perfrectlly fine&lt;/P&gt;</description>
    <pubDate>Sun, 07 Jan 2024 19:14:41 GMT</pubDate>
    <dc:creator>ilanganor1</dc:creator>
    <dc:date>2024-01-07T19:14:41Z</dc:date>
    <item>
      <title>YOcto flash emmc fails</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/YOcto-flash-emmc-fails/m-p/1783972#M18821</link>
      <description>&lt;P&gt;I am building image as such:&lt;/P&gt;&lt;P&gt;export MACHINE=imx8mqevk&lt;BR /&gt;DISTRO=fsl-imx-wayland MACHINE=${MACHINE} source imx-setup-release.sh&lt;/P&gt;&lt;P&gt;andflash using :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;sudo ./uuu -b emmc_all imx-boot-imx8mqevk-sd.bin-flash_evk core-image-base-imx8mqevk.wic.bz2&lt;/P&gt;&lt;P&gt;device do not print anything on boot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;to test I flashed the demo image:&amp;nbsp;&lt;/P&gt;&lt;P&gt;sudo ./uuu -b emmc_all imx-image-full-imx8mpevk.wic&lt;BR /&gt;&lt;BR /&gt;which works perfrectlly fine&lt;/P&gt;</description>
      <pubDate>Sun, 07 Jan 2024 19:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/YOcto-flash-emmc-fails/m-p/1783972#M18821</guid>
      <dc:creator>ilanganor1</dc:creator>
      <dc:date>2024-01-07T19:14:41Z</dc:date>
    </item>
    <item>
      <title>Re: YOcto flash emmc fails</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/YOcto-flash-emmc-fails/m-p/1784944#M18822</link>
      <description>&lt;P&gt;it seems that you didn't download the correct own image, try to find .wic.zst image, if you still couldn't find it, sent your built image list to me, let me tell you which one you use&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 06:46:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/YOcto-flash-emmc-fails/m-p/1784944#M18822</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-01-09T06:46:06Z</dc:date>
    </item>
    <item>
      <title>Re: YOcto flash emmc fails</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/YOcto-flash-emmc-fails/m-p/1785716#M18823</link>
      <description>&lt;P&gt;ok issue found&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for the evk, I needed to build for machine type&amp;nbsp;imx8mpevk and not&amp;nbsp;imx8mqevk as I originally built&lt;BR /&gt;&lt;BR /&gt;I was abble to flash well using this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;sudo ./uuu -b emmc_all imx-boot core-image-base-imx8mpevk.wic.zst&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 04:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/YOcto-flash-emmc-fails/m-p/1785716#M18823</guid>
      <dc:creator>ilanganor1</dc:creator>
      <dc:date>2024-01-10T04:02:35Z</dc:date>
    </item>
  </channel>
</rss>