<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX kernal data pool pointer triggers a Busfault and a Hardfault in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-kernal-data-pool-pointer-triggers-a-Busfault-and-a-Hardfault/m-p/1722127#M18808</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;We have a Firmware that uses MQX RTOS on an &lt;LI-PRODUCT title="iMXRT1024" id="iMXRT1024"&gt;&lt;/LI-PRODUCT&gt;CAG4A when we jump to the address of the firmware a busfault (IMPRECISERR(2)) and a Hardfault (FORCED (0)) gets triggered&lt;BR /&gt;I found out that this happens exactly at this line:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;kernel_data-&amp;gt;KD_POOL = (MEMPOOL_STRUCT_PTR)_mem_create_pool(start, (_mem_size)kernel_data-&amp;gt;INIT.END_OF_KERNEL_MEMORY - (_mem_size)start);&lt;/LI-CODE&gt;&lt;P&gt;we are sure that the jump to the firmware happened because when we prevent the previous line from executing (using while(1) before the line for exemple) we don't get the faults.&lt;BR /&gt;the way I flash the board is I flash with the release image of the firmware then I start a debug session with the debug image of the boodloader.&lt;BR /&gt;&lt;BR /&gt;faults screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="OM120_0-1694611701567.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240837i33BCF3AA1171746D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="OM120_0-1694611701567.png" alt="OM120_0-1694611701567.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;OM120_0-1694611701567.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Firmware linker file:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="OM120_1-1694611786768.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240838i05EB99E273220648/image-size/medium?v=v2&amp;amp;px=400" role="button" title="OM120_1-1694611786768.png" alt="OM120_1-1694611786768.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;OM120_1-1694611786768.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Also when I put the firmware at the start of the flash and run it directly without our bootloader it works without the faults, keep in mind that we tested the bootloader with other applications and it works.&lt;BR /&gt;&lt;BR /&gt;thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Sep 2023 13:55:13 GMT</pubDate>
    <dc:creator>OM120</dc:creator>
    <dc:date>2023-09-13T13:55:13Z</dc:date>
    <item>
      <title>MQX kernal data pool pointer triggers a Busfault and a Hardfault</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-kernal-data-pool-pointer-triggers-a-Busfault-and-a-Hardfault/m-p/1722127#M18808</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;We have a Firmware that uses MQX RTOS on an &lt;LI-PRODUCT title="iMXRT1024" id="iMXRT1024"&gt;&lt;/LI-PRODUCT&gt;CAG4A when we jump to the address of the firmware a busfault (IMPRECISERR(2)) and a Hardfault (FORCED (0)) gets triggered&lt;BR /&gt;I found out that this happens exactly at this line:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;kernel_data-&amp;gt;KD_POOL = (MEMPOOL_STRUCT_PTR)_mem_create_pool(start, (_mem_size)kernel_data-&amp;gt;INIT.END_OF_KERNEL_MEMORY - (_mem_size)start);&lt;/LI-CODE&gt;&lt;P&gt;we are sure that the jump to the firmware happened because when we prevent the previous line from executing (using while(1) before the line for exemple) we don't get the faults.&lt;BR /&gt;the way I flash the board is I flash with the release image of the firmware then I start a debug session with the debug image of the boodloader.&lt;BR /&gt;&lt;BR /&gt;faults screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="OM120_0-1694611701567.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240837i33BCF3AA1171746D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="OM120_0-1694611701567.png" alt="OM120_0-1694611701567.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;OM120_0-1694611701567.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Firmware linker file:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="OM120_1-1694611786768.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240838i05EB99E273220648/image-size/medium?v=v2&amp;amp;px=400" role="button" title="OM120_1-1694611786768.png" alt="OM120_1-1694611786768.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;OM120_1-1694611786768.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Also when I put the firmware at the start of the flash and run it directly without our bootloader it works without the faults, keep in mind that we tested the bootloader with other applications and it works.&lt;BR /&gt;&lt;BR /&gt;thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 13:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-kernal-data-pool-pointer-triggers-a-Busfault-and-a-Hardfault/m-p/1722127#M18808</guid>
      <dc:creator>OM120</dc:creator>
      <dc:date>2023-09-13T13:55:13Z</dc:date>
    </item>
    <item>
      <title>Re: MQX kernal data pool pointer triggers a Busfault and a Hardfault</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-kernal-data-pool-pointer-triggers-a-Busfault-and-a-Hardfault/m-p/1724402#M18810</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;For your question,&amp;nbsp;I would suggest you contact &lt;A href="mailto:mqxsales@nxp.com" target="_blank"&gt;mqxsales@nxp.com&lt;/A&gt;&amp;nbsp;for help.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 18 Sep 2023 04:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-kernal-data-pool-pointer-triggers-a-Busfault-and-a-Hardfault/m-p/1724402#M18810</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2023-09-18T04:57:25Z</dc:date>
    </item>
  </channel>
</rss>