<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Routing RTCS to separate modem in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1235062#M18611</link>
    <description>&lt;P&gt;Hi Daniel&lt;/P&gt;&lt;P&gt;Thank you for this. My understanding is that there needs to be an interface to associate with the default gateway that you propose adding. If I understand your suggestion correctly, as my RTCS stack has only one physical interface, I must therefore create a 'virtual' interface to associate with the default gateway, within which the exchange of datagrams between the two stacks takes place.&lt;BR /&gt;Have I understood correctly?&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;</description>
    <pubDate>Tue, 23 Feb 2021 15:26:48 GMT</pubDate>
    <dc:creator>dnfuss1</dc:creator>
    <dc:date>2021-02-23T15:26:48Z</dc:date>
    <item>
      <title>Routing RTCS to separate modem</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1229871#M18606</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have a product where internet connectivity is already being provided by a modem, whose network stack allows direct access to ip-level traffic.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have recently added ethernet LAN connectivity to this product using RTCS (v4.2.0.2) and a PHY and are looking for an efficient way to route LAN traffic to/from the modem.&lt;/P&gt;&lt;P&gt;I'd be grateful for suggestions as to how this might be best achieved- e.g. can we send/receive data directly at the IP/Network layer within RTCS (akin to a router), or can this only be achieved higher-up the stack via sockets, etc..&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 12:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1229871#M18606</guid>
      <dc:creator>dnfuss1</dc:creator>
      <dc:date>2021-02-11T12:45:22Z</dc:date>
    </item>
    <item>
      <title>Re: Routing RTCS to separate modem</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1234111#M18609</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is a RTCS example&amp;nbsp; demonstrates the gateway feature of the RTCS TCP/IP stack.&lt;/P&gt;
&lt;P&gt;Freescale_MQX_4_2\rtcs\examples\shell&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To add a gateway to the routing table, use the "gate &amp;lt;gateway&amp;gt; [&amp;lt;netaddr&amp;gt; &amp;lt;netmask&amp;gt;]" command.&lt;/P&gt;
&lt;P&gt;For example:&lt;/P&gt;
&lt;P&gt;shell&amp;gt; gate 192.168.0.5&lt;BR /&gt;Adding gateway 192.168.0.5, ip address: 0.0.0.0, netmask: 0.0.0.0&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 05:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1234111#M18609</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2021-02-22T05:42:34Z</dc:date>
    </item>
    <item>
      <title>Re: Routing RTCS to separate modem</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1235062#M18611</link>
      <description>&lt;P&gt;Hi Daniel&lt;/P&gt;&lt;P&gt;Thank you for this. My understanding is that there needs to be an interface to associate with the default gateway that you propose adding. If I understand your suggestion correctly, as my RTCS stack has only one physical interface, I must therefore create a 'virtual' interface to associate with the default gateway, within which the exchange of datagrams between the two stacks takes place.&lt;BR /&gt;Have I understood correctly?&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 15:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1235062#M18611</guid>
      <dc:creator>dnfuss1</dc:creator>
      <dc:date>2021-02-23T15:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: Routing RTCS to separate modem</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1254775#M18626</link>
      <description>&lt;P&gt;I think you have two interfaces:&lt;/P&gt;
&lt;P&gt;--GPRS (PPP)&lt;/P&gt;
&lt;P&gt;--Ethernet&lt;/P&gt;</description>
      <pubDate>Wed, 31 Mar 2021 07:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Routing-RTCS-to-separate-modem/m-p/1254775#M18626</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2021-03-31T07:18:10Z</dc:date>
    </item>
  </channel>
</rss>