<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: work with MQX interrupt in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/work-with-MQX-interrupt/m-p/1152464#M18528</link>
    <description>&lt;P&gt;For an MQX based application, if an interrupt routine is enabled and then a higher priority interrupt comes-- the higher priority interrupt will be handled first?&lt;/P&gt;</description>
    <pubDate>Sun, 13 Sep 2020 14:01:04 GMT</pubDate>
    <dc:creator>davidzhu</dc:creator>
    <dc:date>2020-09-13T14:01:04Z</dc:date>
    <item>
      <title>work with MQX interrupt</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/work-with-MQX-interrupt/m-p/1152463#M18527</link>
      <description>&lt;P&gt;Hi support:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the preemption of interrupts with higher priority still valid with the use of MQX in the application?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 13 Sep 2020 13:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/work-with-MQX-interrupt/m-p/1152463#M18527</guid>
      <dc:creator>davidzhu</dc:creator>
      <dc:date>2020-09-13T13:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: work with MQX interrupt</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/work-with-MQX-interrupt/m-p/1152464#M18528</link>
      <description>&lt;P&gt;For an MQX based application, if an interrupt routine is enabled and then a higher priority interrupt comes-- the higher priority interrupt will be handled first?&lt;/P&gt;</description>
      <pubDate>Sun, 13 Sep 2020 14:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/work-with-MQX-interrupt/m-p/1152464#M18528</guid>
      <dc:creator>davidzhu</dc:creator>
      <dc:date>2020-09-13T14:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: work with MQX interrupt</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/work-with-MQX-interrupt/m-p/1152552#M18533</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;In MQX user guider ,section 3.9 describes the interrupts and exceptions in MQX.&lt;/P&gt;
&lt;P&gt;The interrupts are still nested on Cortex-M4. MQX itself uses a timer interrupt for BSP tick (5 ms), and many IO drivers use interrupts as well, such as for example serial UART driver or SPI driver, Ethernet, USB, etc.&lt;/P&gt;
&lt;P&gt;The priorities of these interrupts are assigned by the MQX driver, they are BSP dependent.&lt;/P&gt;
&lt;P&gt;MQX also provides a way to bypass MQX kernel with a kernel isr.&lt;/P&gt;
&lt;P&gt;More details, please read MQX user's Guide, 3.9 Handling Interrupts and Exceptions.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 02:51:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/work-with-MQX-interrupt/m-p/1152552#M18533</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-09-14T02:51:33Z</dc:date>
    </item>
  </channel>
</rss>