<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: Flash driver with MQX</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-driver-with-MQX/m-p/1092199#M18514</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MQX&lt;/STRONG&gt;&lt;SPAN&gt; 4.x includes a SPI driver. This driver supports the operation master mode. If enabled in user configuration, the SPI device drivers are installed during the BSP startup code as “spi0:” (or “spiX:” where X is index of the SPI module used). The SPI driver is significantly rewritten in the &lt;STRONG&gt;MQX&lt;/STRONG&gt; 4.0, so &lt;SPAN style="color: black;"&gt;that there is no distinct interrupt or polled driver type. See I/O User Guide for details. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black;"&gt;On Kinetis and Vybrid platforms, the driver uses DMA to function. there is a simpler example application available in MQX, this example shows how to read/write data from/to external SPI EEPROM. Additional HW setup is needed.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black;"&gt;You can find this example at the next path: / mqx/examples/spi &lt;/SPAN&gt;&lt;/P&gt;&lt;PRE style="color: #000000;"&gt;&lt;/PRE&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 May 2020 21:53:35 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2020-05-30T21:53:35Z</dc:date>
    <item>
      <title>Flash driver with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-driver-with-MQX/m-p/1092198#M18513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi support:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my project I need to store data on K70. I want to use an external serial flash memory. Is there any demos available for MQX? or any driver for SPI interface?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 May 2020 21:35:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-driver-with-MQX/m-p/1092198#M18513</guid>
      <dc:creator>antonychen2008</dc:creator>
      <dc:date>2020-05-30T21:35:17Z</dc:date>
    </item>
    <item>
      <title>Re: Flash driver with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-driver-with-MQX/m-p/1092199#M18514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MQX&lt;/STRONG&gt;&lt;SPAN&gt; 4.x includes a SPI driver. This driver supports the operation master mode. If enabled in user configuration, the SPI device drivers are installed during the BSP startup code as “spi0:” (or “spiX:” where X is index of the SPI module used). The SPI driver is significantly rewritten in the &lt;STRONG&gt;MQX&lt;/STRONG&gt; 4.0, so &lt;SPAN style="color: black;"&gt;that there is no distinct interrupt or polled driver type. See I/O User Guide for details. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black;"&gt;On Kinetis and Vybrid platforms, the driver uses DMA to function. there is a simpler example application available in MQX, this example shows how to read/write data from/to external SPI EEPROM. Additional HW setup is needed.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black;"&gt;You can find this example at the next path: / mqx/examples/spi &lt;/SPAN&gt;&lt;/P&gt;&lt;PRE style="color: #000000;"&gt;&lt;/PRE&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 May 2020 21:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-driver-with-MQX/m-p/1092199#M18514</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-05-30T21:53:35Z</dc:date>
    </item>
  </channel>
</rss>