<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: rtcs_shell_twrk60f120m and httpsrv_twrk60f120m in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169900#M1851</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Keith Tang,&lt;/P&gt;&lt;P&gt;I was facing the exact same problem, and I'm very glad that you managed to find the solution.&lt;/P&gt;&lt;P&gt;Thank you so much!&lt;/P&gt;&lt;P&gt;AV&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Mar 2013 14:31:44 GMT</pubDate>
    <dc:creator>alexandrevincon</dc:creator>
    <dc:date>2013-03-20T14:31:44Z</dc:date>
    <item>
      <title>rtcs_shell_twrk60f120m and httpsrv_twrk60f120m</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169898#M1849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have anyone tried running rtcs_shell_twrk60f120m? Does it work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried it briefly and it doesn't seem to work. I&amp;nbsp;stepped through the codes, and found that it fails at obtaining IP address through DHCP. Setting it to manual IP address succeeded (of course!) but it fails to communicate with the remote computer, i.e. I cannot ping the tower.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;tried httpsrv_twrk60f120m as well, it binds the address correctly and seems to be running, but I cannot connect to it, i.e. browsing the IP address via browser fails.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I believe the above two are due to the same RTCS problem. Anyone can shed some lights?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2012 15:17:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169898#M1849</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-06-06T15:17:55Z</dc:date>
    </item>
    <item>
      <title>Re: rtcs_shell_twrk60f120m and httpsrv_twrk60f120m</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169899#M1850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have to say this Freescale forum is really quiet, probably due to the relatively low usage of MQX. Anyway, just to help the new comers like me, here is the answer to the question I posted above.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When you are using TWRK60F120M, it uses RMII interface instead of MII, for whatever reasons. The TWR-SER board, on the other hand, has its default settings set to MII mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hence to change from MII to RMII mode, you need to change the following jumpers setting:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. J2, the CLK_SEL jumper. Short pin 3-4 instead of 1-2. RMII requires 50 MHz to work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. J12, the ETH_CONFIG jumper. Default is left open. You need to insert a jumper across pin 9-10. Please check the PHY KSZ8041NL datasheet on the configuration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2012 18:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169899#M1850</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-06-07T18:00:14Z</dc:date>
    </item>
    <item>
      <title>Re: rtcs_shell_twrk60f120m and httpsrv_twrk60f120m</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169900#M1851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Keith Tang,&lt;/P&gt;&lt;P&gt;I was facing the exact same problem, and I'm very glad that you managed to find the solution.&lt;/P&gt;&lt;P&gt;Thank you so much!&lt;/P&gt;&lt;P&gt;AV&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2013 14:31:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169900#M1851</guid>
      <dc:creator>alexandrevincon</dc:creator>
      <dc:date>2013-03-20T14:31:44Z</dc:date>
    </item>
    <item>
      <title>Re: rtcs_shell_twrk60f120m and httpsrv_twrk60f120m</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169901#M1852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AV and others,&lt;/P&gt;&lt;P&gt;Sorry for the trouble on configuring the hardware.&amp;nbsp; I've been bitten in past too but have learned to consult the FSL_MQX_getting_started.pdf document in the MQX4.0/doc path.&lt;/P&gt;&lt;P&gt;Section 7 has all the default board/tower configuration settings (the release notes also point to this document):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118542iD4912C1116DBDA34/image-size/large?v=v2&amp;amp;px=999" title="ScreenHunter_11 Mar. 20 10.31.gif" alt="ScreenHunter_11 Mar. 20 10.31.gif" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2013 15:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169901#M1852</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2013-03-20T15:35:05Z</dc:date>
    </item>
    <item>
      <title>Re: rtcs_shell_twrk60f120m and httpsrv_twrk60f120m</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169902#M1853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for this precious information.&lt;/P&gt;&lt;P&gt;But it is also a bit confusing, because I think this is hardware related and shall be either in TRWKF120M or TWR-SER user's manual, not MQX !&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;AV&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 07:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169902#M1853</guid>
      <dc:creator>alexandrevincon</dc:creator>
      <dc:date>2013-03-21T07:46:26Z</dc:date>
    </item>
    <item>
      <title>Re: rtcs_shell_twrk60f120m and httpsrv_twrk60f120m</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169903#M1854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AV,&lt;/P&gt;&lt;P&gt;just information not trying to say right or wrong.&lt;/P&gt;&lt;P&gt;The tower mcu card are configured to run all by themselves without the TWR SER card (ie bare metal...no rtos) and to run some default application without any development tool.&lt;/P&gt;&lt;P&gt;Enter MQX...it has been setup run with TWR SER card.&amp;nbsp; It also enables fast prototyping and relatively easy implementation of Ethernet, USB, MZfS, etc.&lt;/P&gt;&lt;P&gt;So MQX is a fundamental part of our enablement. &lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 13:14:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/rtcs-shell-twrk60f120m-and-httpsrv-twrk60f120m/m-p/169903#M1854</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2013-03-21T13:14:23Z</dc:date>
    </item>
  </channel>
</rss>