<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: read/write USB/SD without filesystem</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/read-write-USB-SD-without-filesystem/m-p/1064800#M18489</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB doesn't have the implementation to have a R/W directly without a file system and the conclusion is that it is better for you use SD and explore using the IO driver and using the examples provided in the document MQXIOUG.pdf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We already have an ESDHC driver.This driver defines common interface for communication with various types of cards including SD, SDHC, SDIO etc. The driver is currently used as an alternative to SPI low level communication for SDCARD wrapper under the MFS stack. You can find the example of using the driver in section 16.11 of MQXIOUG.pdf document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regard&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2020 02:47:01 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2020-06-24T02:47:01Z</dc:date>
    <item>
      <title>read/write USB/SD without filesystem</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/read-write-USB-SD-without-filesystem/m-p/1064799#M18488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to access read/write&amp;nbsp; to a Usb Mass storage device directly without a filesystem? I think the overhead of a file system is too big. &lt;/P&gt;&lt;P&gt;I'd like to be able to simple access the entire device with MQX.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jun 2020 22:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/read-write-USB-SD-without-filesystem/m-p/1064799#M18488</guid>
      <dc:creator>davidzhu</dc:creator>
      <dc:date>2020-06-06T22:03:53Z</dc:date>
    </item>
    <item>
      <title>Re: read/write USB/SD without filesystem</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/read-write-USB-SD-without-filesystem/m-p/1064800#M18489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB doesn't have the implementation to have a R/W directly without a file system and the conclusion is that it is better for you use SD and explore using the IO driver and using the examples provided in the document MQXIOUG.pdf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We already have an ESDHC driver.This driver defines common interface for communication with various types of cards including SD, SDHC, SDIO etc. The driver is currently used as an alternative to SPI low level communication for SDCARD wrapper under the MFS stack. You can find the example of using the driver in section 16.11 of MQXIOUG.pdf document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regard&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2020 02:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/read-write-USB-SD-without-filesystem/m-p/1064800#M18489</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-06-24T02:47:01Z</dc:date>
    </item>
  </channel>
</rss>