<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Problems when reading large files from USB stick.</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946772#M18304</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="29824" data-username="m4l490n" href="https://community.nxp.com/people/m4l490n"&gt;Manuel:&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is an MFS filesystem issue, and fixed in MQX 4.2, and patch 4.2.0.2.&amp;nbsp; Please refer to the attached release notes for the MFS bug fix.&lt;/P&gt;&lt;P&gt;I would suggest you update to MQX 4.2.0 + patch if possible.&lt;/P&gt;&lt;P&gt;Or you can try to merger the new MFS part to your project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Oct 2019 06:01:05 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2019-10-24T06:01:05Z</dc:date>
    <item>
      <title>Problems when reading large files from USB stick.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946769#M18301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm facing problems when reading large files. I have some code that copies one file from a USB stick to an SD Card. But I'm facing issues when copying large files, larger than 10MB. Here is how I'm doing it:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;I open the file I want to copy in the "source" media as "r"&lt;/LI&gt;&lt;LI&gt;I open a file on the "dest" device with attributes as "wb"&lt;/LI&gt;&lt;LI&gt;I allocate an 8192 byte buffer that is the one I will use for reading from the source file and writing to the destination file.&lt;/LI&gt;&lt;LI&gt;I read 8192 bytes from the source file and write them to the destination file. I do this as many times as bytes there are.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Everything goes well for the first couple of megs, but then randomly, the "read" function returns 0 and the source device stops responding, even when I close the file and try to open it again. I have done this copying successfully with files under 10 MB but it doesn't work with files larger than that. I'm reading from USB and immediately writing to the SD Card without interruption or delays, I don't know if I need to introduce a delay in between read and write or something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I'm trying to know if this is the correct way of doing it, just opening both files, read from one and write to the other. I mean, it works just fine for files up to 10MB so I'm not sure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Oct 2019 13:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946769#M18301</guid>
      <dc:creator>m4l490n</dc:creator>
      <dc:date>2019-10-21T13:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: Problems when reading large files from USB stick.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946770#M18302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please let me know your MQX version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2019 12:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946770#M18302</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-10-23T12:34:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problems when reading large files from USB stick.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946771#M18303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/danielchen@fsl"&gt;danielchen@fsl&lt;/A&gt;‌ my MQX version is 4.1.1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2019 14:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946771#M18303</guid>
      <dc:creator>m4l490n</dc:creator>
      <dc:date>2019-10-23T14:55:13Z</dc:date>
    </item>
    <item>
      <title>Re: Problems when reading large files from USB stick.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946772#M18304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="29824" data-username="m4l490n" href="https://community.nxp.com/people/m4l490n"&gt;Manuel:&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is an MFS filesystem issue, and fixed in MQX 4.2, and patch 4.2.0.2.&amp;nbsp; Please refer to the attached release notes for the MFS bug fix.&lt;/P&gt;&lt;P&gt;I would suggest you update to MQX 4.2.0 + patch if possible.&lt;/P&gt;&lt;P&gt;Or you can try to merger the new MFS part to your project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2019 06:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problems-when-reading-large-files-from-USB-stick/m-p/946772#M18304</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-10-24T06:01:05Z</dc:date>
    </item>
  </channel>
</rss>