<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックUSB-Bluetooth Adapter</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Bluetooth-Adapter/m-p/169136#M1784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have the 52259 demo board, with codewarrior 7.1 and Freescale MQX 3.0. my task is to connect Wiimote to the board and i imagine one the solutions for this is the USB-Bluetooth adapter (the other might be using the Ethernet interface of the board but i'm still not sure how close Ethernet and bluetooth are and how difficult it is to do)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so for start i need some driver for connecting a USB-Bluetooth adapter to the board..as i've understood there is no support for this in the existing libraries though there might be support for low-level functions...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so any suggestions? anywhere i can find the driver i need? or should i go through writing the driver myself?!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jan 2010 08:37:53 GMT</pubDate>
    <dc:creator>Babak</dc:creator>
    <dc:date>2010-01-21T08:37:53Z</dc:date>
    <item>
      <title>USB-Bluetooth Adapter</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Bluetooth-Adapter/m-p/169136#M1784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have the 52259 demo board, with codewarrior 7.1 and Freescale MQX 3.0. my task is to connect Wiimote to the board and i imagine one the solutions for this is the USB-Bluetooth adapter (the other might be using the Ethernet interface of the board but i'm still not sure how close Ethernet and bluetooth are and how difficult it is to do)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so for start i need some driver for connecting a USB-Bluetooth adapter to the board..as i've understood there is no support for this in the existing libraries though there might be support for low-level functions...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so any suggestions? anywhere i can find the driver i need? or should i go through writing the driver myself?!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2010 08:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Bluetooth-Adapter/m-p/169136#M1784</guid>
      <dc:creator>Babak</dc:creator>
      <dc:date>2010-01-21T08:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: USB-Bluetooth Adapter</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Bluetooth-Adapter/m-p/169137#M1785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Babak. Unfortunatelly, no such driver is written in MQX yet.&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by JuroV on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2010-02-08&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;09:45 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2010 16:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Bluetooth-Adapter/m-p/169137#M1785</guid>
      <dc:creator>JuroV</dc:creator>
      <dc:date>2010-02-08T16:45:20Z</dc:date>
    </item>
  </channel>
</rss>