<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックExit Shell from program</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Exit-Shell-from-program/m-p/754554#M17763</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a way to exit a Shell Task via a programming command?&lt;/P&gt;&lt;P&gt;I have a shell task, which is essentially&amp;nbsp;just a while(1) loop with the shell command inside the loop.&lt;/P&gt;&lt;P&gt;I can enter the exit command from the keyboard, but I would like to cause the shell to exit and restart with a programming statement. Issuing Shell_exit causes the system to crash/lockup.&lt;/P&gt;&lt;P&gt;I am doing this because I'd like to change the commands available to the end user.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Apr 2018 11:47:21 GMT</pubDate>
    <dc:creator>markdoxbeck</dc:creator>
    <dc:date>2018-04-21T11:47:21Z</dc:date>
    <item>
      <title>Exit Shell from program</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Exit-Shell-from-program/m-p/754554#M17763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a way to exit a Shell Task via a programming command?&lt;/P&gt;&lt;P&gt;I have a shell task, which is essentially&amp;nbsp;just a while(1) loop with the shell command inside the loop.&lt;/P&gt;&lt;P&gt;I can enter the exit command from the keyboard, but I would like to cause the shell to exit and restart with a programming statement. Issuing Shell_exit causes the system to crash/lockup.&lt;/P&gt;&lt;P&gt;I am doing this because I'd like to change the commands available to the end user.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Apr 2018 11:47:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Exit-Shell-from-program/m-p/754554#M17763</guid>
      <dc:creator>markdoxbeck</dc:creator>
      <dc:date>2018-04-21T11:47:21Z</dc:date>
    </item>
    <item>
      <title>Re: Exit Shell from program</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Exit-Shell-from-program/m-p/754555#M17764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark：&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest you try to terminate the shell task.&lt;/P&gt;&lt;P&gt;MQX RTOS frees task resources, when it terminates a task.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 May 2018 08:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Exit-Shell-from-program/m-p/754555#M17764</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2018-05-16T08:32:34Z</dc:date>
    </item>
  </channel>
</rss>