<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MQX 4.2 SAI driver issue in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SAI-driver-issue/m-p/747958#M17750</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ryan:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, please refer to the _io_sai_dma_install function,&amp;nbsp;&amp;nbsp; poiner &amp;nbsp; io_read and pointer &amp;nbsp; io_write are null.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30655iFA8CC1252C3A09C3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Mar 2018 06:29:08 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2018-03-19T06:29:08Z</dc:date>
    <item>
      <title>MQX 4.2 SAI driver issue</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SAI-driver-issue/m-p/747957#M17749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use the SAI driver with MQX 4.2. Looking at the dai_dma_demo example project it seems as simple as calling fopen on the SAI driver and then a call to write. Both of these functions take an MQX_FILE_PTR. It appears that fopen sets up the MQX_FILE_PTR struct but the pointers to IO_WRITE/READ in that struct are null after a call to fopen. I can't find anything in the example code that sets up these function pointers. Are they null because I'm using DMA? Calling write returns MQX_IO_OPERATION_NOT_AVAILABLE&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Mar 2018 23:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SAI-driver-issue/m-p/747957#M17749</guid>
      <dc:creator>ryanlush</dc:creator>
      <dc:date>2018-03-10T23:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: MQX 4.2 SAI driver issue</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SAI-driver-issue/m-p/747958#M17750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ryan:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, please refer to the _io_sai_dma_install function,&amp;nbsp;&amp;nbsp; poiner &amp;nbsp; io_read and pointer &amp;nbsp; io_write are null.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30655iFA8CC1252C3A09C3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Mar 2018 06:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SAI-driver-issue/m-p/747958#M17750</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2018-03-19T06:29:08Z</dc:date>
    </item>
  </channel>
</rss>