<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR-SER2 Ethernet in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747804#M17746</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Priya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The TWR-SER2 has an (old) National Instruments / Texas Instruments DP83849I PHY, which is a dual port PHY used to connect two Ethernet controllers to two Ethernet ports. Since the K60 has only one interface you can only use one of the Ethernet ports.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What you need is a switch, such as the Micrel KSZ8863, which is a three-port PHY/switch but allows connecting just one Ethernet controller to two Ethernet ports. This allows the PHY to operate as a switch (saving the need for a Hub/external switch) and also allows (with tail-tagging mode) one Ethernet controller to act as two separate Ethernet ports on different IP addresses or networks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This functionality is included in the Open Source uTasker K60 project and an overview can be found in &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fdocs%2FuTasker%2FuTaskerNetworking.pdf" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/uTasker/uTaskerNetworking.pdf&lt;/A&gt;&lt;SPAN&gt; - see especially the appendix B which details the KSZ8863 tail-tagging mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Nov 2017 13:30:13 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2017-11-04T13:30:13Z</dc:date>
    <item>
      <title>TWR-SER2 Ethernet</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747803#M17745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on TWR-K60F120M tower board and TWR-SER2 for Ethernet Connectivity.&lt;/P&gt;&lt;P&gt;I am able to establish connectivity with ETH-A port (using MQX RTOS demo code eth_to_serial).&lt;/P&gt;&lt;P&gt;Now, my requirement is to create a daisy chain Ethernet switch as below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16618i9BDA299EA09435DA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Due to less ports on Ethernet HUB, I want to provide Ethernet connectivity to PC via TWR-SER2 board.&lt;/P&gt;&lt;P&gt;Can anyone please let me know, is it possible to implement this using TWR boards?&lt;/P&gt;&lt;P&gt;How can I achieve the same? Will there be any update on transceiver driver files(dp83xxxx.c and dp83xxxx.h).&lt;/P&gt;&lt;P&gt;What implementation needed on K60 side?&lt;/P&gt;&lt;P&gt;As its my first time with ethernet, please help me by clarifying my concepts.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Nov 2017 14:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747803#M17745</guid>
      <dc:creator>priyagupta</dc:creator>
      <dc:date>2017-11-03T14:48:24Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-SER2 Ethernet</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747804#M17746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Priya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The TWR-SER2 has an (old) National Instruments / Texas Instruments DP83849I PHY, which is a dual port PHY used to connect two Ethernet controllers to two Ethernet ports. Since the K60 has only one interface you can only use one of the Ethernet ports.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What you need is a switch, such as the Micrel KSZ8863, which is a three-port PHY/switch but allows connecting just one Ethernet controller to two Ethernet ports. This allows the PHY to operate as a switch (saving the need for a Hub/external switch) and also allows (with tail-tagging mode) one Ethernet controller to act as two separate Ethernet ports on different IP addresses or networks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This functionality is included in the Open Source uTasker K60 project and an overview can be found in &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fdocs%2FuTasker%2FuTaskerNetworking.pdf" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/uTasker/uTaskerNetworking.pdf&lt;/A&gt;&lt;SPAN&gt; - see especially the appendix B which details the KSZ8863 tail-tagging mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Nov 2017 13:30:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747804#M17746</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-11-04T13:30:13Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-SER2 Ethernet</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747805#M17747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply.&amp;nbsp;I would like to know, how can I implement the&amp;nbsp;switch with '&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;KSZ8863&lt;/SPAN&gt;' without uTasker..&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need driver files for 'KSZ8863', which I can include in bsp_twrk60f120m/enet/phy project.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Nov 2017 19:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747805#M17747</guid>
      <dc:creator>priyagupta</dc:creator>
      <dc:date>2017-11-06T19:29:34Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-SER2 Ethernet</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747806#M17748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can either copy the code from the files in the uTasker project or write your own to do the same thing.&lt;BR /&gt;For MQX you can contact MQX to see whether they sell an extension for your requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 09:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/TWR-SER2-Ethernet/m-p/747806#M17748</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-11-07T09:09:27Z</dc:date>
    </item>
  </channel>
</rss>