<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: MQX 4.2 &amp; Quad SPI driver</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Quad-SPI-driver/m-p/715827#M17604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Blue:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you can change the IO mode in the QuadSPI_INIT_STRUCT.&lt;/P&gt;&lt;P&gt;you also can use IOCTL command to do that.&lt;/P&gt;&lt;P&gt;ioctl(qspifd, QuadSPI_IOCTL_SET_QUAD_IO, NULL);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Dec 2017 07:47:01 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2017-12-18T07:47:01Z</dc:date>
    <item>
      <title>MQX 4.2 &amp; Quad SPI driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Quad-SPI-driver/m-p/715826#M17603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as I have seen the default settings of the quad spi driver of MQX is set in single mode:&lt;/P&gt;&lt;P&gt;init_qspi.c&lt;/P&gt;&lt;P&gt;static const QuadSPI_INIT_STRUCT _bsp_quadspi1_init_data = {&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; QuadSPI_CLK_SDR_MODE,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Clock Mode */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; QuadSPI_SINGLE_MODE,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* IO Mode */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 33000000,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Serial Clock: Read */&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;I would like now to set it into quad mode. I am not sure if it is enough only change the IO mode into "QuadSPI_QUAD_MODE".&lt;/P&gt;&lt;P&gt;Does someone have experience about it, or can someone give me hints about the settings for quad spi driver. I use the quad-spi 2 of VF3xx.&lt;/P&gt;&lt;P&gt;Many thanks in advance for any hints.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2017 14:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Quad-SPI-driver/m-p/715826#M17603</guid>
      <dc:creator>BlueJay</dc:creator>
      <dc:date>2017-12-12T14:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: MQX 4.2 &amp; Quad SPI driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Quad-SPI-driver/m-p/715827#M17604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Blue:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you can change the IO mode in the QuadSPI_INIT_STRUCT.&lt;/P&gt;&lt;P&gt;you also can use IOCTL command to do that.&lt;/P&gt;&lt;P&gt;ioctl(qspifd, QuadSPI_IOCTL_SET_QUAD_IO, NULL);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Dec 2017 07:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Quad-SPI-driver/m-p/715827#M17604</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-12-18T07:47:01Z</dc:date>
    </item>
    <item>
      <title>Re: MQX 4.2 &amp; Quad SPI driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Quad-SPI-driver/m-p/715828#M17605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your reply.&lt;/P&gt;&lt;P&gt;Yes, there is init data structure :_bsp_quadspi1_init_data&lt;/P&gt;&lt;P&gt;The IO mode Needs to be changed into Quad mode&lt;/P&gt;&lt;P&gt;In additional the _bsp_quadspi1_flash_cmd needs to be updated also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Bluejay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 09:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Quad-SPI-driver/m-p/715828#M17605</guid>
      <dc:creator>BlueJay</dc:creator>
      <dc:date>2018-01-17T09:44:17Z</dc:date>
    </item>
  </channel>
</rss>