<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FreeRTOS adapter for Freescale USB stack 5.0? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/FreeRTOS-adapter-for-Freescale-USB-stack-5-0/m-p/710255#M17583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm&amp;nbsp;still using the v5.0 beta of the Freescale BM USB stack and I'm curious if there's an RTOS adapter for it already written for FreeRTOS.&amp;nbsp; I realize it's deprecated but switching to KSDK and MCUXpresso is simply not an option right now - I've got deadlines to meet and that's going to be hard enough without switching tools in the middle of everything.&amp;nbsp; It's working well enough now but I see that it supports running as a task in MQX, and if I can do the same in FreeRTOS to reduce the amount of processing done in interrupt context, that would be useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Oct 2017 15:45:59 GMT</pubDate>
    <dc:creator>scottm</dc:creator>
    <dc:date>2017-10-18T15:45:59Z</dc:date>
    <item>
      <title>FreeRTOS adapter for Freescale USB stack 5.0?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/FreeRTOS-adapter-for-Freescale-USB-stack-5-0/m-p/710255#M17583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm&amp;nbsp;still using the v5.0 beta of the Freescale BM USB stack and I'm curious if there's an RTOS adapter for it already written for FreeRTOS.&amp;nbsp; I realize it's deprecated but switching to KSDK and MCUXpresso is simply not an option right now - I've got deadlines to meet and that's going to be hard enough without switching tools in the middle of everything.&amp;nbsp; It's working well enough now but I see that it supports running as a task in MQX, and if I can do the same in FreeRTOS to reduce the amount of processing done in interrupt context, that would be useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Oct 2017 15:45:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/FreeRTOS-adapter-for-Freescale-USB-stack-5-0/m-p/710255#M17583</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2017-10-18T15:45:59Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS adapter for Freescale USB stack 5.0?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/FreeRTOS-adapter-for-Freescale-USB-stack-5-0/m-p/710256#M17584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="266884" data-username="scottm" href="https://community.nxp.com/people/scottm"&gt;SCOTT MILLER&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KSDK USB is based on usb 5.0, I would suggest you refer to the adapter files for FreeRTOS, these files are from KSDK1.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6369i5AB48DA9477C7AE7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Oct 2017 08:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/FreeRTOS-adapter-for-Freescale-USB-stack-5-0/m-p/710256#M17584</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-10-26T08:53:54Z</dc:date>
    </item>
  </channel>
</rss>