<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: k64 cpu with mqx4.1 uart issue in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/k64-cpu-with-mqx4-1-uart-issue/m-p/692087#M17482</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Daniel,&lt;/P&gt;&lt;P&gt;Thank you for your reply, and I have checked the UARTx_C1 register:&lt;/P&gt;&lt;P&gt;ODD: 0x13&lt;/P&gt;&lt;P&gt;EVEN: 0x12&lt;/P&gt;&lt;P&gt;It seems right, but when I do the test, it is the same when setting even or odd.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jul 2017 09:22:39 GMT</pubDate>
    <dc:creator>wulinweng</dc:creator>
    <dc:date>2017-07-17T09:22:39Z</dc:date>
    <item>
      <title>k64 cpu with mqx4.1 uart issue</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/k64-cpu-with-mqx4-1-uart-issue/m-p/692085#M17480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;I used K64 CPU with MQX4.1, When I used UART in my project, baud rate is setting to 115200, and the issue is if I set the parity to odd, the even/odd parity of my software&amp;nbsp;can both connect to my device which is k64.&lt;/P&gt;&lt;P&gt;and if I set the device parity to even, the odd/even parity of my PC software can both connect to the device too.&lt;/P&gt;&lt;P&gt;Can you show me what's the problem, I think it is bsp of the mqx4.1 issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 07:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/k64-cpu-with-mqx4-1-uart-issue/m-p/692085#M17480</guid>
      <dc:creator>wulinweng</dc:creator>
      <dc:date>2017-07-11T07:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: k64 cpu with mqx4.1 uart issue</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/k64-cpu-with-mqx4-1-uart-issue/m-p/692086#M17481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi wulin:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest you check the UARTx_C1 register to get the real value for parity check first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25071i23DD61577C4B09A3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 13:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/k64-cpu-with-mqx4-1-uart-issue/m-p/692086#M17481</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-07-13T13:50:16Z</dc:date>
    </item>
    <item>
      <title>Re: k64 cpu with mqx4.1 uart issue</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/k64-cpu-with-mqx4-1-uart-issue/m-p/692087#M17482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Daniel,&lt;/P&gt;&lt;P&gt;Thank you for your reply, and I have checked the UARTx_C1 register:&lt;/P&gt;&lt;P&gt;ODD: 0x13&lt;/P&gt;&lt;P&gt;EVEN: 0x12&lt;/P&gt;&lt;P&gt;It seems right, but when I do the test, it is the same when setting even or odd.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jul 2017 09:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/k64-cpu-with-mqx4-1-uart-issue/m-p/692087#M17482</guid>
      <dc:creator>wulinweng</dc:creator>
      <dc:date>2017-07-17T09:22:39Z</dc:date>
    </item>
  </channel>
</rss>