<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: RTCS configuration on Vybrid</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682452#M17408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At start of connection the pc see that eth link is up and send many packages for UPnP devices, NetBIOS and SSDP (windows standard services). My application use an proprietary UDP socket to communicate with the target. At startup i send and rcv packages with 60 Byte length.&lt;/P&gt;&lt;P&gt;After that i start continous datatransfer with packages up to 1060 bytes length between pc and target.&lt;/P&gt;&lt;P&gt;If i start these communication many of these packages are lost. My pc application repeated these frames but if the other messages (UPnP and so on) are tranmitted by windows it will lost.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Jul 2017 09:44:50 GMT</pubDate>
    <dc:creator>m68000</dc:creator>
    <dc:date>2017-07-06T09:44:50Z</dc:date>
    <item>
      <title>RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682444#M17400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Im using first time RTCS to communicate over UDP. So far, it work's fine.&lt;/P&gt;&lt;P&gt;But when i start the communication between PC and target with RTCS and any other frames&lt;/P&gt;&lt;P&gt;like dhcp or zeroconf transmitted by PC, all further transmission stops.&lt;/P&gt;&lt;P&gt;My data packets don't receive by RTCS in these case.&lt;/P&gt;&lt;P&gt;If no other communication is active, all packets received by RTCS.&lt;/P&gt;&lt;P&gt;I think the problem is, that these frames received, but no one consume the request.&lt;/P&gt;&lt;P&gt;As result if UDP frames transmitted by PC, no memory avilable and RTCS lost frames.&lt;/P&gt;&lt;P&gt;My configuration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; _RTCSPCB_init = 8;&lt;BR /&gt;&amp;nbsp; _RTCSPCB_grow = 2;&lt;BR /&gt;&amp;nbsp; _RTCSPCB_max = 40;&lt;BR /&gt;&amp;nbsp; _RTCS_msgpool_init = 4;&lt;BR /&gt;&amp;nbsp; _RTCS_msgpool_grow = 2;&lt;BR /&gt;&amp;nbsp; _RTCS_msgpool_max&amp;nbsp; = 20;&lt;BR /&gt;&amp;nbsp; _RTCS_socket_part_init = 4;&lt;BR /&gt;&amp;nbsp; _RTCS_socket_part_grow = 2;&lt;BR /&gt;&amp;nbsp; _RTCS_socket_part_max&amp;nbsp; = 20;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Changing RTCS priorty (default in my system: 6) to higher level, no changes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2017 04:07:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682444#M17400</guid>
      <dc:creator>m68000</dc:creator>
      <dc:date>2017-07-05T04:07:53Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682445#M17401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefan:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Zero-configuration network is not implemented in RTCS stack. But DHCP should work. Did you get the assigned IP address from the DHCP server?&lt;/P&gt;&lt;P&gt;There is a DHCP example in MQX_RTCS_User_Guide.pdf.&amp;nbsp; Page 225. You can refer to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2017 07:22:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682445#M17401</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-07-05T07:22:26Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682446#M17402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in my project i use a static ip address.&lt;/P&gt;&lt;P&gt;I think my problem is that after start of my connection many frames like MDNS, SSDP ….&lt;/P&gt;&lt;P&gt;transmitted by the pc tot he target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RTCS receive all these frames and have to procced them. If RTCS has not enough memory&lt;/P&gt;&lt;P&gt;my frames cannot received.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it right?&lt;/P&gt;&lt;P&gt;What can i do to change these?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Von: danielchen@fsl &lt;/P&gt;&lt;P&gt;Gesendet: Mittwoch, 5. Juli 2017 09:23&lt;/P&gt;&lt;P&gt;An: R+T - Stefan Lammert &amp;lt;stefan.lammert@rxt.de&amp;gt;&lt;/P&gt;&lt;P&gt;Betreff: Re:  - Re: RTCS configuration on Vybrid&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: RTCS configuration on Vybrid&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Daniel Chen&amp;lt;https://community.nxp.com/people/danielchen@fsl?et=watches.email.thread&amp;gt; in MQX Software Solutions - View the full discussion&amp;lt;https://community.nxp.com/message/920789?commentID=920789&amp;amp;et=watches.email.thread#comment-920789&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2017 10:31:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682446#M17402</guid>
      <dc:creator>m68000</dc:creator>
      <dc:date>2017-07-05T10:31:23Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682447#M17403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefan:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I think you can try to increase the RTCS init parameters. Especially RTCS_xxx_max. Please also check the following document for RTCS parameters introduction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-102077"&gt;https://community.nxp.com/docs/DOC-102077&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 02:52:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682447#M17403</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-07-06T02:52:33Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682448#M17404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i readed this document before i have posted my problem.&lt;/P&gt;&lt;P&gt;RTCS has many flags and properties to configure. In Example, i have all values that are described doubled, but&lt;/P&gt;&lt;P&gt;no changes.&lt;/P&gt;&lt;P&gt;Use RTCS queues to store incoming messages? What are there lifetime? Discard RTCS not supported received messages&amp;nbsp; (e.g.SSDP messages (this is UDP))?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 07:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682448#M17404</guid>
      <dc:creator>m68000</dc:creator>
      <dc:date>2017-07-06T07:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682449#M17405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In case the queue is full and a new incoming packet comes, it is discarded.&lt;/P&gt;&lt;P&gt;SSDP uses UDP transport protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 08:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682449#M17405</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-07-06T08:22:05Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682450#M17406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the result, if i increase the value _UDP_max_queue_size ,BSPCFG_RX_RING_LEN&amp;nbsp;&amp;nbsp; and BSPCFG_TX_RING_LEN?&lt;/P&gt;&lt;P&gt;Let these values the udp queue grows up?&lt;/P&gt;&lt;P&gt;How can i delete unused packets on the rx queue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 08:28:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682450#M17406</guid>
      <dc:creator>m68000</dc:creator>
      <dc:date>2017-07-06T08:28:54Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682451#M17407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you increase the value of ,BSPCFG_RX_RING_LEN and BSPCFG_TX_RING_LEN, the enet driver will handle more packets at one time.&amp;nbsp; _UDP_max_queue_size is the maximum number of packets that will be enqueued.&lt;/P&gt;&lt;P&gt;Of course your system will consume more memory.&lt;/P&gt;&lt;P&gt;I don't think there is a good way to delete or drop unused packets on the rx queue in RTCS stack.&lt;/P&gt;&lt;P&gt;Is there a huge traffic between your board and PC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 09:27:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682451#M17407</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-07-06T09:27:36Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS configuration on Vybrid</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682452#M17408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At start of connection the pc see that eth link is up and send many packages for UPnP devices, NetBIOS and SSDP (windows standard services). My application use an proprietary UDP socket to communicate with the target. At startup i send and rcv packages with 60 Byte length.&lt;/P&gt;&lt;P&gt;After that i start continous datatransfer with packages up to 1060 bytes length between pc and target.&lt;/P&gt;&lt;P&gt;If i start these communication many of these packages are lost. My pc application repeated these frames but if the other messages (UPnP and so on) are tranmitted by windows it will lost.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 09:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-configuration-on-Vybrid/m-p/682452#M17408</guid>
      <dc:creator>m68000</dc:creator>
      <dc:date>2017-07-06T09:44:50Z</dc:date>
    </item>
  </channel>
</rss>