<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SD card writing after ejection in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-writing-after-ejection/m-p/656700#M17265</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've a problem with SD card writing.&lt;/P&gt;&lt;P&gt;The installation of SD card is ok, from esdhc to mfs over partition, as indicated in \mfs\examples\sdcard\demo.c, and I can write properly a file with the demo command "sd write".&lt;/P&gt;&lt;P&gt;But if I remove and then insert again the SD card,&amp;nbsp;the "sd write" command gives me the answer "Error writing file...". With "sd dir" the file seems to be on the filesystem, but when I restart the device, that file is not there.&amp;nbsp;I also tried&amp;nbsp;to change cache mode with MFS_WRITE_THROUGH_CACHE, but the problem remains.&lt;/P&gt;&lt;P&gt;I saw similar topics about SD card writing, but no one can help me.&lt;/P&gt;&lt;P&gt;Maybe I need to reinstall filesystem again?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Jan 2017 13:57:00 GMT</pubDate>
    <dc:creator>mircopizzichini</dc:creator>
    <dc:date>2017-01-03T13:57:00Z</dc:date>
    <item>
      <title>SD card writing after ejection</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-writing-after-ejection/m-p/656700#M17265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've a problem with SD card writing.&lt;/P&gt;&lt;P&gt;The installation of SD card is ok, from esdhc to mfs over partition, as indicated in \mfs\examples\sdcard\demo.c, and I can write properly a file with the demo command "sd write".&lt;/P&gt;&lt;P&gt;But if I remove and then insert again the SD card,&amp;nbsp;the "sd write" command gives me the answer "Error writing file...". With "sd dir" the file seems to be on the filesystem, but when I restart the device, that file is not there.&amp;nbsp;I also tried&amp;nbsp;to change cache mode with MFS_WRITE_THROUGH_CACHE, but the problem remains.&lt;/P&gt;&lt;P&gt;I saw similar topics about SD card writing, but no one can help me.&lt;/P&gt;&lt;P&gt;Maybe I need to reinstall filesystem again?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 13:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-writing-after-ejection/m-p/656700#M17265</guid>
      <dc:creator>mircopizzichini</dc:creator>
      <dc:date>2017-01-03T13:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: SD card writing after ejection</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-writing-after-ejection/m-p/656701#M17266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a quick check about this demo with Frdm-k64, I can see there is a "SD card uninstalled " info when you remove SD card and "Installing MFS over partition ..." when you reinsert SD card.&amp;nbsp; So I can write successfully again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13774i545498B1143928D3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your issue, it seems that MFS not installed correctly before you write a file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2017 04:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-writing-after-ejection/m-p/656701#M17266</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-02-13T04:53:48Z</dc:date>
    </item>
  </channel>
</rss>