<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX USB port vs FTDI interfaces? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-port-vs-FTDI-interfaces/m-p/656415#M17264</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a CDC communications device that is running "MQX Vitual Com Demo" and I need a USB host bridge to connect it to another micros UART.&amp;nbsp; For some reason I can not connect to it using any of the FTDI products.&amp;nbsp; I am being told by them it is not "standard"&amp;nbsp; I have also tried several other USB bridge devices with no luck. I can get them to enumerate and connect but can never get my data to transfer. &amp;nbsp; I can connect to it via the PC though.&amp;nbsp;&amp;nbsp; The device manufacture comes up as "Freescale Semiconductor inc" and the product description as "MQX Virtual Com Demo"....VID = 0x2504 and PID = 0x300.&amp;nbsp; There are 3 end points...0x81 in/interrupt, 0x82 in/Bulk and 0x83 out/Bulk.&amp;nbsp; Any idea what the issue is???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jan 2017 12:17:34 GMT</pubDate>
    <dc:creator>paulmateer</dc:creator>
    <dc:date>2017-01-31T12:17:34Z</dc:date>
    <item>
      <title>MQX USB port vs FTDI interfaces?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-port-vs-FTDI-interfaces/m-p/656415#M17264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a CDC communications device that is running "MQX Vitual Com Demo" and I need a USB host bridge to connect it to another micros UART.&amp;nbsp; For some reason I can not connect to it using any of the FTDI products.&amp;nbsp; I am being told by them it is not "standard"&amp;nbsp; I have also tried several other USB bridge devices with no luck. I can get them to enumerate and connect but can never get my data to transfer. &amp;nbsp; I can connect to it via the PC though.&amp;nbsp;&amp;nbsp; The device manufacture comes up as "Freescale Semiconductor inc" and the product description as "MQX Virtual Com Demo"....VID = 0x2504 and PID = 0x300.&amp;nbsp; There are 3 end points...0x81 in/interrupt, 0x82 in/Bulk and 0x83 out/Bulk.&amp;nbsp; Any idea what the issue is???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jan 2017 12:17:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-port-vs-FTDI-interfaces/m-p/656415#M17264</guid>
      <dc:creator>paulmateer</dc:creator>
      <dc:date>2017-01-31T12:17:34Z</dc:date>
    </item>
  </channel>
</rss>