<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX 4.2 SPI Master/Slave: first frame received with delay in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SPI-Master-Slave-first-frame-received-with-delay/m-p/646469#M17133</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm implementing a SPI slave module for the Kinetis K60FX512, running with MQX 4.2 (I'm using the new SPI drivers in full-duplex mode). To test it I've set up a SPI master and a slave on different SPIx accesses, each running on a dedicated task, and connected the pins externally and set-up a very slow clock (5 KHz).&lt;/P&gt;&lt;P&gt;The slave prepares its transmit buffer, and the spi driver eventually calls the _dspi_tx_rx() function, that pushes it to the bus and blocks (it is configured to use ISR) until the&amp;nbsp;message from the master is received.&lt;/P&gt;&lt;P&gt;After that the master is initialized, prepares its transmit buffer, and the function&amp;nbsp;&lt;SPAN&gt;_dspi_tx_rx() pushes it to the bus and simultaneously tries to read what the slave sent. The problem is that nothing on the first frame is transmitted by the slave, instead the first frame sent by the slave is only transmitted during the execution of the second frame. All further frames are then transmitted by the slave with a delay of one (the last frame of each message is sent as the first of the following) - see attached picture. This does not happen in the other direction, i.e. the master sends its frames on time, and are thus read timely by the slave.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I've compared the behaviour with another application where the K60 controls as a master an external peripheral, and this does not happen, i.e. the first frame from the slave is received as the first frame from the master is sent. I've tried to manually match the register configuration of both cases at the entrance of the&amp;nbsp;_dspi_tx_rx() function, to no avail.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Any tips to solve this problem would be gratly appreciated. Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Goncalo.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SPI Configuration:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Master:&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SPI0,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SPI MODE 0 (CPHA=0, CPOL =0),&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;8 bit Frame size,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BIG ENDIAN&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CS=0 (I control the CS pin manually),&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;0xFFFFFFFF Dummy pattern,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;DMA Disabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Slave: SPI2,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SPI MODE 0 (CPHA=0, CPOL =0),&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;8 bit Frame size,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BIG ENDIAN&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;USE ISR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CS=0,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;0xFFFFFFFF Dummy pattern,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;DMA Disabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Attachement 1: First message transmitted on SPI bus. CH1: SCK, CH2: MISO. (Slave TXBUFF: 0x55 0x55 0x55 0x55)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Attachement 2: SPI register contents at end of first message transmitted (Just before master returns from _dspi_tx_rx() ).Master: SPI0, Slave SPI2. Master sends: 0x41 0x00 0x00 0x00. Slave sends: 0x01, 0x02 0x03 0x04.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jan 2017 11:48:38 GMT</pubDate>
    <dc:creator>goncaloandre</dc:creator>
    <dc:date>2017-01-26T11:48:38Z</dc:date>
    <item>
      <title>MQX 4.2 SPI Master/Slave: first frame received with delay</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SPI-Master-Slave-first-frame-received-with-delay/m-p/646469#M17133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm implementing a SPI slave module for the Kinetis K60FX512, running with MQX 4.2 (I'm using the new SPI drivers in full-duplex mode). To test it I've set up a SPI master and a slave on different SPIx accesses, each running on a dedicated task, and connected the pins externally and set-up a very slow clock (5 KHz).&lt;/P&gt;&lt;P&gt;The slave prepares its transmit buffer, and the spi driver eventually calls the _dspi_tx_rx() function, that pushes it to the bus and blocks (it is configured to use ISR) until the&amp;nbsp;message from the master is received.&lt;/P&gt;&lt;P&gt;After that the master is initialized, prepares its transmit buffer, and the function&amp;nbsp;&lt;SPAN&gt;_dspi_tx_rx() pushes it to the bus and simultaneously tries to read what the slave sent. The problem is that nothing on the first frame is transmitted by the slave, instead the first frame sent by the slave is only transmitted during the execution of the second frame. All further frames are then transmitted by the slave with a delay of one (the last frame of each message is sent as the first of the following) - see attached picture. This does not happen in the other direction, i.e. the master sends its frames on time, and are thus read timely by the slave.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I've compared the behaviour with another application where the K60 controls as a master an external peripheral, and this does not happen, i.e. the first frame from the slave is received as the first frame from the master is sent. I've tried to manually match the register configuration of both cases at the entrance of the&amp;nbsp;_dspi_tx_rx() function, to no avail.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Any tips to solve this problem would be gratly appreciated. Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Goncalo.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SPI Configuration:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Master:&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SPI0,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SPI MODE 0 (CPHA=0, CPOL =0),&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;8 bit Frame size,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BIG ENDIAN&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CS=0 (I control the CS pin manually),&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;0xFFFFFFFF Dummy pattern,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;DMA Disabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Slave: SPI2,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SPI MODE 0 (CPHA=0, CPOL =0),&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;8 bit Frame size,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BIG ENDIAN&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;USE ISR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CS=0,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;0xFFFFFFFF Dummy pattern,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;DMA Disabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Attachement 1: First message transmitted on SPI bus. CH1: SCK, CH2: MISO. (Slave TXBUFF: 0x55 0x55 0x55 0x55)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Attachement 2: SPI register contents at end of first message transmitted (Just before master returns from _dspi_tx_rx() ).Master: SPI0, Slave SPI2. Master sends: 0x41 0x00 0x00 0x00. Slave sends: 0x01, 0x02 0x03 0x04.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2017 11:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SPI-Master-Slave-first-frame-received-with-delay/m-p/646469#M17133</guid>
      <dc:creator>goncaloandre</dc:creator>
      <dc:date>2017-01-26T11:48:38Z</dc:date>
    </item>
    <item>
      <title>Re: MQX 4.2 SPI Master/Slave: first frame received with delay</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SPI-Master-Slave-first-frame-received-with-delay/m-p/646470#M17134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please let me know which BSP are you using?&lt;/P&gt;&lt;P&gt;Is it possible to reproduce this issue in a NXP board?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2017 23:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-SPI-Master-Slave-first-frame-received-with-delay/m-p/646470#M17134</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-02-15T23:26:40Z</dc:date>
    </item>
  </channel>
</rss>