<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Simultaneous SDCard Access Corruption</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Simultaneous-SDCard-Access-Corruption/m-p/618217#M16892</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I am patched through 4.2.0.2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 May 2017 14:33:52 GMT</pubDate>
    <dc:creator>leifzars</dc:creator>
    <dc:date>2017-05-01T14:33:52Z</dc:date>
    <item>
      <title>Simultaneous SDCard Access Corruption</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Simultaneous-SDCard-Access-Corruption/m-p/618215#M16890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The project is set up as follows. USB with MSC access to the SDCard&amp;nbsp;device, along with MFS on top of the SDCard as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I know that it is potentially unsafe for both USB and MFS to access&amp;nbsp;to the SDCard simultaneously, but in this case USB is only reading, while MFS both reads and writes.&amp;nbsp;So I know of no reason&amp;nbsp;why this is not acceptable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the board boots it starts a self test, writing a few hundred K to a file via MFS and then reading it back to validate. The writing appears to go fine, but the reading randomly fails in random ways. MFS reports no issue but the data is invalid. The odd thing is that when I attempt an immediate re read of the data (1 block of 512 bytes) it is valid. Now this only happens when Windows is scanning / reading the SDCard via USB MSC, and I verified that no writes are being issued via MSC. So as&amp;nbsp;soon as a compile out the MSC support or unplug the USB cable the self test works every time with no re reading necessary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So some portion of the SDCard driver, or sub driver is being corrupted. I am not overly familiar with this driver,&amp;nbsp;so I am asking for some guidance. Anyone have an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leif&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2017 13:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Simultaneous-SDCard-Access-Corruption/m-p/618215#M16890</guid>
      <dc:creator>leifzars</dc:creator>
      <dc:date>2017-04-18T13:33:35Z</dc:date>
    </item>
    <item>
      <title>Re: Simultaneous SDCard Access Corruption</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Simultaneous-SDCard-Access-Corruption/m-p/618216#M16891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leif:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which MQX version you are using?&lt;/P&gt;&lt;P&gt;Not sure what is the root cause now. But if you are using an older version, I would suggest you update to the latest version, MQX 4.2.0 and plus the patch 4.2.0.2. Because this version fixed one important MFS issue.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14062i9F8F56EA5FF653C6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please refer to the release note for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 03:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Simultaneous-SDCard-Access-Corruption/m-p/618216#M16891</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-04-25T03:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: Simultaneous SDCard Access Corruption</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Simultaneous-SDCard-Access-Corruption/m-p/618217#M16892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I am patched through 4.2.0.2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 May 2017 14:33:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Simultaneous-SDCard-Access-Corruption/m-p/618217#M16892</guid>
      <dc:creator>leifzars</dc:creator>
      <dc:date>2017-05-01T14:33:52Z</dc:date>
    </item>
  </channel>
</rss>