<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can't Go From Dynamic IP to Static IP in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612722#M16814</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I put ipcfg_bind_dhcp_wait() in a separate task to avoid code delays; and it worked.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm note sure why the ipcfg_unbind() constantly returns 7425 (1D01 hex) in my above code, but I'm under a project deadline so I have to move on.&amp;nbsp; Thank you for your replies.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Sep 2016 20:42:55 GMT</pubDate>
    <dc:creator>kackle123</dc:creator>
    <dc:date>2016-09-26T20:42:55Z</dc:date>
    <item>
      <title>Can't Go From Dynamic IP to Static IP</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612717#M16809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question very similar to this unanswered question:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/315763"&gt;https://community.nxp.com/thread/315763&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I am using MQX 4.2.0.1 on a K64.&amp;nbsp; Using an embedded web page, I tell the K64 to go from its static IP address, to a dynamic, and then back to a static.&amp;nbsp; The program uses the ipcfg functions, but won't go from a dynamic address back to a static address.&amp;nbsp; The ipcfg_unbind() constantly returns 7425 (1D01 hex), even if I call it repeatedly.&amp;nbsp; When debugging deeper, there seems to be some semaphore problem within ipcfg.c.&amp;nbsp; Is this something someone can recreate on their end?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Sep 2016 21:10:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612717#M16809</guid>
      <dc:creator>kackle123</dc:creator>
      <dc:date>2016-09-12T21:10:38Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Go From Dynamic IP to Static IP</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612718#M16810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I did a quick test with shell commands, with demo&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_2\rtcs\examples\shell\build\iar\rtcs_shell_frdmk64f&lt;/P&gt;&lt;P&gt;My test result is it can go from dynamic ip to static ip in my side.&lt;/P&gt;&lt;P&gt;Could you please double check it? Please see the below picutre&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5041i0365D77435C58BC5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 04:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612718#M16810</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2016-09-13T04:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Go From Dynamic IP to Static IP</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612719#M16811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you; I will try it and post my results here.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 18:11:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612719#M16811</guid>
      <dc:creator>kackle123</dc:creator>
      <dc:date>2016-09-19T18:11:07Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Go From Dynamic IP to Static IP</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612720#M16812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried the MQX shell example project.&amp;nbsp; It worked.&amp;nbsp; I noticed it uses ipcfg_bind_dhcp_wait().&amp;nbsp; My code was trying to use ipcfg_bind_dhcp() instead; can you confirm that ipcfg_bind_dhcp() works when using ipcfg_bind_staticip() later?&amp;nbsp; (Code snippet attached.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 20:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612720#M16812</guid>
      <dc:creator>kackle123</dc:creator>
      <dc:date>2016-09-21T20:03:31Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Go From Dynamic IP to Static IP</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612721#M16813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ipcfg_bind_dhcp :&amp;nbsp; Binds Ethernet device to networking using DHCP protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ipcfg_bind_dhcp_wait :&amp;nbsp; Bind Ethernet device to network using a DHCP protocol, blocking mode.&amp;nbsp;&amp;nbsp; This function will not return until the process is finished or error occures.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As the DHCP address resolving make take some time. I suggest you using&amp;nbsp; ipcfg_bind_dhcp_wait().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 03:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612721#M16813</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2016-09-22T03:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Go From Dynamic IP to Static IP</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612722#M16814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I put ipcfg_bind_dhcp_wait() in a separate task to avoid code delays; and it worked.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm note sure why the ipcfg_unbind() constantly returns 7425 (1D01 hex) in my above code, but I'm under a project deadline so I have to move on.&amp;nbsp; Thank you for your replies.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 20:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Can-t-Go-From-Dynamic-IP-to-Static-IP/m-p/612722#M16814</guid>
      <dc:creator>kackle123</dc:creator>
      <dc:date>2016-09-26T20:42:55Z</dc:date>
    </item>
  </channel>
</rss>