<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: PPP pver serial</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/PPP-pver-serial/m-p/604527#M16733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think PPP assumes that you have a multi thread OS. There are some interaction between tcp/ip and ppp threads.&amp;nbsp; It will be not easy to implement it without OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Nov 2016 08:45:44 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2016-11-22T08:45:44Z</dc:date>
    <item>
      <title>PPP pver serial</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/PPP-pver-serial/m-p/604526#M16732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to use the PPP over the serial port. I would like to avoid the usage of the operating system.&lt;/P&gt;&lt;P&gt;The example attached in SDK are using the MQX. Is it so necessary ?&lt;/P&gt;&lt;P&gt;If I use the bare metal structure, will it be so expensive to process in the loop ?&lt;/P&gt;&lt;P&gt;I have other things running in the main loop, I am not in a critical situation now, but I don t know if the addition of the&lt;/P&gt;&lt;P&gt;LWIP will be so straightforward. I will also need to process few sockets open. I need an idea of how much is possible to do&lt;/P&gt;&lt;P&gt;without using the operating system..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 08:35:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/PPP-pver-serial/m-p/604526#M16732</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2016-10-04T08:35:04Z</dc:date>
    </item>
    <item>
      <title>Re: PPP pver serial</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/PPP-pver-serial/m-p/604527#M16733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think PPP assumes that you have a multi thread OS. There are some interaction between tcp/ip and ppp threads.&amp;nbsp; It will be not easy to implement it without OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 08:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/PPP-pver-serial/m-p/604527#M16733</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2016-11-22T08:45:44Z</dc:date>
    </item>
  </channel>
</rss>