<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX v4.2 with VLE in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-v4-2-with-VLE/m-p/598107#M16647</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I work with an MPC5644A MCU, which has an e200z4 dual issue core. &lt;BR /&gt;&lt;SPAN&gt;Can I compile the MQX v4.2 to VLE instructions? According to the linked doc (&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fassets%2Fdocuments%2Fdata%2Fen%2Fsupporting-information%2FFSL_MQX_4_0_2_RN.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/assets/documents/data/en/supporting-information/FSL_MQX_4_0_2_RN.pdf&lt;/A&gt;&lt;SPAN&gt; ), MQX is ported to e200 VLE, so I think it should work, but it doesn't. When the execution reaches the _mqx() function, it jumps to the Interrupt section and stucks. The first intruction in the _mqx() function is se_stb r2,4(rsp). &lt;/SPAN&gt;&lt;BR /&gt;Although I'm not sure, that the problem is about the VLE instructions...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help in this topic is appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;BR /&gt;János Murai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2017 14:17:12 GMT</pubDate>
    <dc:creator>janos_murai</dc:creator>
    <dc:date>2017-02-03T14:17:12Z</dc:date>
    <item>
      <title>MQX v4.2 with VLE</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-v4-2-with-VLE/m-p/598107#M16647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I work with an MPC5644A MCU, which has an e200z4 dual issue core. &lt;BR /&gt;&lt;SPAN&gt;Can I compile the MQX v4.2 to VLE instructions? According to the linked doc (&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fassets%2Fdocuments%2Fdata%2Fen%2Fsupporting-information%2FFSL_MQX_4_0_2_RN.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/assets/documents/data/en/supporting-information/FSL_MQX_4_0_2_RN.pdf&lt;/A&gt;&lt;SPAN&gt; ), MQX is ported to e200 VLE, so I think it should work, but it doesn't. When the execution reaches the _mqx() function, it jumps to the Interrupt section and stucks. The first intruction in the _mqx() function is se_stb r2,4(rsp). &lt;/SPAN&gt;&lt;BR /&gt;Although I'm not sure, that the problem is about the VLE instructions...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help in this topic is appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;BR /&gt;János Murai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 14:17:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-v4-2-with-VLE/m-p/598107#M16647</guid>
      <dc:creator>janos_murai</dc:creator>
      <dc:date>2017-02-03T14:17:12Z</dc:date>
    </item>
    <item>
      <title>Re: MQX v4.2 with VLE</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-v4-2-with-VLE/m-p/598108#M16648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately MQX 4.2 does not support PowerPC devices. &lt;BR /&gt;You need to use MQX4.0.2. this is the lastest version that supports PowerPC devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 22:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-v4-2-with-VLE/m-p/598108#M16648</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-02-07T22:43:27Z</dc:date>
    </item>
    <item>
      <title>Re: MQX v4.2 with VLE</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-v4-2-with-VLE/m-p/598109#M16649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi soledad, did you use mqx4.0.2 for PowerPC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 07:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-v4-2-with-VLE/m-p/598109#M16649</guid>
      <dc:creator>burakduzgun</dc:creator>
      <dc:date>2018-02-22T07:13:47Z</dc:date>
    </item>
  </channel>
</rss>