<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Which KSDK2.0 drivers API can be used in FreeRTOS task</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Which-KSDK2-0-drivers-API-can-be-used-in-FreeRTOS-task/m-p/592534#M16611</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Selected drivers provide FreeRTOS support in form of an additional layer, however it is possible to use the KSDK bare metal drivers.&lt;/P&gt;&lt;P&gt;You can find an example in this link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332257"&gt;HOW TO USE LPTMR KSDK DRIVER IN A FREERTOS PROJECT&lt;/A&gt; &lt;/P&gt;&lt;P&gt;I hope it helps!!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jul 2016 18:19:58 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2016-07-25T18:19:58Z</dc:date>
    <item>
      <title>Which KSDK2.0 drivers API can be used in FreeRTOS task</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Which-KSDK2-0-drivers-API-can-be-used-in-FreeRTOS-task/m-p/592533#M16610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to use KSDK2.0 drivers with FreeRTOS on K22F.&lt;/P&gt;&lt;P&gt;I search in the community but i found nothing about compatibility between KSDK2.0 API drivers and FreeRTOS.&lt;/P&gt;&lt;P&gt;I only found in the community that it is possible to use KDSK2.0 GPIO drivers in FreeRTOS task but nothing more on all others SDK2.0 drivers.&lt;/P&gt;&lt;P&gt;In the drivers folder, the only drivers labelled "FreeRTOS" are :&lt;/P&gt;&lt;P&gt;DSPI with "fsl_dspi_freertos.h"&lt;/P&gt;&lt;P&gt;I2C with&amp;nbsp;&amp;nbsp;&amp;nbsp; "fsl_i2c_freertos.h"&lt;/P&gt;&lt;P&gt;LPUART with "fsl_lpuart_freertos.h"&lt;/P&gt;&lt;P&gt;UART with "fsl_uart_freertos.h"&lt;/P&gt;&lt;P&gt;That is very limitative, that mean that we can't use ADC, DAC, CMP, TIMERS, FLASH, FTM, PIT, WDOG.&lt;/P&gt;&lt;P&gt;in FreeRTOS tasks ?&lt;/P&gt;&lt;P&gt;In this case even if FreeRTOS is free, i can't use it, because i can only use DSP,UART an I2C ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The most incomprehensive is that community say that GPIO can be use in FreeRTOS task but it is not labelled "fsl_gpio_freertos.h" ?&lt;/P&gt;&lt;P&gt;Please can you say me where is the logic ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the "SDK_2.0.FRDM-K22F\boards\frdmk22f"&amp;nbsp; I found only FreeRTOS drivers in "rtos_examples".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question is : can i use&amp;nbsp; KSDK2.0 drivers in FreeRTOS task ? or i can only use FreeRTOS drivers in FreeRTOS task ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is anybody can help&amp;nbsp; to &lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;clarify the question ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 14:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Which-KSDK2-0-drivers-API-can-be-used-in-FreeRTOS-task/m-p/592533#M16610</guid>
      <dc:creator>didierjeanjean</dc:creator>
      <dc:date>2016-06-30T14:41:33Z</dc:date>
    </item>
    <item>
      <title>Re: Which KSDK2.0 drivers API can be used in FreeRTOS task</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Which-KSDK2-0-drivers-API-can-be-used-in-FreeRTOS-task/m-p/592534#M16611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Selected drivers provide FreeRTOS support in form of an additional layer, however it is possible to use the KSDK bare metal drivers.&lt;/P&gt;&lt;P&gt;You can find an example in this link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332257"&gt;HOW TO USE LPTMR KSDK DRIVER IN A FREERTOS PROJECT&lt;/A&gt; &lt;/P&gt;&lt;P&gt;I hope it helps!!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 18:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Which-KSDK2-0-drivers-API-can-be-used-in-FreeRTOS-task/m-p/592534#M16611</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-07-25T18:19:58Z</dc:date>
    </item>
  </channel>
</rss>