<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 _timer_cancel()</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/timer-cancel/m-p/587242#M16602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm using MQX 4.2.2 and I have a problem with _timer_cancel() function call.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm calling _timer_cancel(id) within the timer's callback itself and it seems that MQX do not find myself and delete me from the scheduled timers in the system. The same function call, called outside the timer's callback works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - can _timer_cancel() be called inside the timer's callback itself or we need to call the function outside the timer ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Alessandro.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jun 2016 13:35:19 GMT</pubDate>
    <dc:creator>alessandrobiasc</dc:creator>
    <dc:date>2016-06-29T13:35:19Z</dc:date>
    <item>
      <title>_timer_cancel()</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/timer-cancel/m-p/587242#M16602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm using MQX 4.2.2 and I have a problem with _timer_cancel() function call.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm calling _timer_cancel(id) within the timer's callback itself and it seems that MQX do not find myself and delete me from the scheduled timers in the system. The same function call, called outside the timer's callback works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - can _timer_cancel() be called inside the timer's callback itself or we need to call the function outside the timer ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Alessandro.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 13:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/timer-cancel/m-p/587242#M16602</guid>
      <dc:creator>alessandrobiasc</dc:creator>
      <dc:date>2016-06-29T13:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: _timer_cancel()</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/timer-cancel/m-p/587243#M16603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alessandro,&lt;/P&gt;&lt;P&gt;With my testing of the _timer_cancel() it too does not work from within the callback but does work when outside the callback.&lt;/P&gt;&lt;P&gt;Please cancel timer outside of the callback.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;PS&lt;/P&gt;&lt;P&gt;I ran test using C:\Freescale\Freescale_MQX_4_2\mqx\examples\timer for frdm-k64f using CW10.6.&lt;/P&gt;&lt;P&gt;main.c attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 16:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/timer-cancel/m-p/587243#M16603</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2016-06-29T16:44:49Z</dc:date>
    </item>
  </channel>
</rss>