<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックADC MUX runtime support in TWRK60F120M</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166807#M1660</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can someone tell me if ADC MUX runtime is supported in TWRK60F120M? I checked through the BSP files, and found that the muxsel parameter within the ADC structure (defined in adc_kadc_prv.h) is only used once in the _adc_hw_channel_init() function of the adc_kadc.c file, to select either channel A or B during hardware initialisation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am expecting to see a runtime function to alternate between channel A and B, i.e. when the value of A channel is read, it switches to B channel for the next conversion, and vice versa. However I don't see any such function in the BSP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please tell me if this is the case, as I need to be sure that I can use ADC0_SE7A and ADC0_SE7B at the same time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 26 May 2012 13:15:39 GMT</pubDate>
    <dc:creator>keithtang</dc:creator>
    <dc:date>2012-05-26T13:15:39Z</dc:date>
    <item>
      <title>ADC MUX runtime support in TWRK60F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166807#M1660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can someone tell me if ADC MUX runtime is supported in TWRK60F120M? I checked through the BSP files, and found that the muxsel parameter within the ADC structure (defined in adc_kadc_prv.h) is only used once in the _adc_hw_channel_init() function of the adc_kadc.c file, to select either channel A or B during hardware initialisation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am expecting to see a runtime function to alternate between channel A and B, i.e. when the value of A channel is read, it switches to B channel for the next conversion, and vice versa. However I don't see any such function in the BSP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please tell me if this is the case, as I need to be sure that I can use ADC0_SE7A and ADC0_SE7B at the same time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 May 2012 13:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166807#M1660</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-05-26T13:15:39Z</dc:date>
    </item>
    <item>
      <title>Re: ADC MUX runtime support in TWRK60F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166808#M1661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello keith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there's no runtime function to your needs. How did you resolve your issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MartinK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Nov 2012 07:25:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166808#M1661</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2012-11-13T07:25:43Z</dc:date>
    </item>
    <item>
      <title>Re: ADC MUX runtime support in TWRK60F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166809#M1662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Too bad, I had to write my own custom API for that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2012 02:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166809#M1662</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-11-14T02:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: ADC MUX runtime support in TWRK60F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166810#M1663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HeLLo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you share code snippet with community? It could help users if they run into same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MartinK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2012 06:07:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166810#M1663</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2012-11-14T06:07:34Z</dc:date>
    </item>
    <item>
      <title>Re: ADC MUX runtime support in TWRK60F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166811#M1664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will have to check with my project leader, as this is a customised project for our client who owns the right to the development.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2012 06:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166811#M1664</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-11-14T06:47:57Z</dc:date>
    </item>
    <item>
      <title>Re: ADC MUX runtime support in TWRK60F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166812#M1665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith,&lt;/P&gt;&lt;P&gt;If you can share just the small portion without compromising your customer that would be great.&amp;nbsp; Since MQX is free and the community really is setup to help one another the more we share the better for all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a great appnote that might also be helpful to you and others.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.google.com/url?sa=t&amp;amp;rct=j&amp;amp;q=freescale%20an4590&amp;amp;source=web&amp;amp;cd=1&amp;amp;cad=rja&amp;amp;ved=0CDoQFjAA&amp;amp;url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fapp_note%2FAN4590.pdf&amp;amp;ei=B8OjUM_HOeiK2wWo0oCYBA&amp;amp;usg=AFQjCNGNmF4-ckUKytva1zqjXTeMpj9_4Q"&gt;AN4590 Using DMA to Emulate ADC Flexible Scan Mode on Kinetis K Series&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A great search tool for appnotes, docs, example code for appnotes is:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/infocenter/index.jsp"&gt;http://www.freescale.com/infocenter/index.jsp&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Just enter keyword in search box.&lt;/P&gt;&lt;P&gt;The AN4590 is pretty new and not certain why it is not found but I'll pass that onto the web folk.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2012 16:16:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/ADC-MUX-runtime-support-in-TWRK60F120M/m-p/166812#M1665</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2012-11-14T16:16:28Z</dc:date>
    </item>
  </channel>
</rss>