<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 MQX_CHECK_VALIDITY</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CHECK-VALIDITY/m-p/546019#M16467</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have a general question about the code executed if MQX_CHECK_VALIDITY is set.&lt;/P&gt;&lt;P&gt;This is an example of _lwsem_post from MQX 4.2.2 :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_1467881894828131 jive_macro_code jive_text_macro" data-renderedposition="132.40000915527344_50_798_240" jivemacro_uid="_1467881894828131"&gt;&lt;P&gt;_mqx_uint _lwsem_post&lt;/P&gt;&lt;P&gt;(&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LWSEM_STRUCT_PTR sem_ptr&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;{ /* Body */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* ...... */&lt;/P&gt;&lt;P&gt;#if MQX_CHECK_VALIDITY&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (sem_ptr-&amp;gt;VALID != LWSEM_VALID)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _KLOGX2(KLOG_lwsem_post, MQX_INVALID_LWSEM);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return (MQX_INVALID_LWSEM);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } /* Endif */&lt;/P&gt;&lt;P&gt;#endif /* MQX_CHECK_VALIDITY */&lt;/P&gt;&lt;P&gt;/* ...... */&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Why this code is executed without any kind of mutual exclusion (mutex, interrupt disable, ...) ? The current task can be preempted during the check and another task can "validate/invalidate" the lwsem. I'm missing something in the implementation (sorry for this) ?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Alessandro.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Jul 2016 09:01:23 GMT</pubDate>
    <dc:creator>alessandrobiasc</dc:creator>
    <dc:date>2016-07-07T09:01:23Z</dc:date>
    <item>
      <title>MQX_CHECK_VALIDITY</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CHECK-VALIDITY/m-p/546019#M16467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have a general question about the code executed if MQX_CHECK_VALIDITY is set.&lt;/P&gt;&lt;P&gt;This is an example of _lwsem_post from MQX 4.2.2 :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_1467881894828131 jive_macro_code jive_text_macro" data-renderedposition="132.40000915527344_50_798_240" jivemacro_uid="_1467881894828131"&gt;&lt;P&gt;_mqx_uint _lwsem_post&lt;/P&gt;&lt;P&gt;(&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LWSEM_STRUCT_PTR sem_ptr&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;{ /* Body */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* ...... */&lt;/P&gt;&lt;P&gt;#if MQX_CHECK_VALIDITY&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (sem_ptr-&amp;gt;VALID != LWSEM_VALID)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _KLOGX2(KLOG_lwsem_post, MQX_INVALID_LWSEM);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return (MQX_INVALID_LWSEM);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } /* Endif */&lt;/P&gt;&lt;P&gt;#endif /* MQX_CHECK_VALIDITY */&lt;/P&gt;&lt;P&gt;/* ...... */&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Why this code is executed without any kind of mutual exclusion (mutex, interrupt disable, ...) ? The current task can be preempted during the check and another task can "validate/invalidate" the lwsem. I'm missing something in the implementation (sorry for this) ?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Alessandro.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 09:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CHECK-VALIDITY/m-p/546019#M16467</guid>
      <dc:creator>alessandrobiasc</dc:creator>
      <dc:date>2016-07-07T09:01:23Z</dc:date>
    </item>
    <item>
      <title>Re: MQX_CHECK_VALIDITY</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CHECK-VALIDITY/m-p/546020#M16468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alessandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, this code is executed with interrupt disable, it is wrapped in the macro.&amp;nbsp; Please check the macro _KLOGX2 defines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define _KLOGX2(fn,p1) _KLOG(_klog_log(KLOG_FUNCTION_EXIT, \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; (_mqx_max_type)(fn), (_mqx_max_type)(p1), (_mqx_max_type)0, (_mqx_max_type)0, (_mqx_max_type)0);)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void _klog_log&lt;/P&gt;&lt;P&gt;(&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mqx_uint type,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mqx_max_type p1,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mqx_max_type p2,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mqx_max_type p3,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mqx_max_type p4,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mqx_max_type p5&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;{ /* Body */&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;_INT_DISABLE();&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;_lwlog_write(LOG_KERNEL_LOG_NUMBER, (_mqx_max_type)type, p1, p2, p3, p4, p5,&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;calling_pc);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;_INT_ENABLE();&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 22:22:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CHECK-VALIDITY/m-p/546020#M16468</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2016-07-07T22:22:20Z</dc:date>
    </item>
  </channel>
</rss>