<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: often not start oscillation MK10DN128VLH5</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531196#M16419</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX 4.2 doesn't support the MK10DN128VLH5 device so I assume you are cloning the twr-k20d50m bsp, is it correct??&lt;/P&gt;&lt;P&gt;If you are using the same clock configuration then you don't need to modify the bsp_cm.c file, however if you need made some modification then you need to follow the attached document, this &lt;SPAN lang="EN-US"&gt;document that explains how to change the default clock configurations.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Aug 2016 20:53:28 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2016-08-16T20:53:28Z</dc:date>
    <item>
      <title>often not start oscillation MK10DN128VLH5</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531195#M16418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The circuit is same as TWR-K20D50M&lt;/P&gt;&lt;P&gt;Resonator : CSTCE8M00G55-R0&lt;/P&gt;&lt;P&gt;Rf : 1 meg ohm&lt;/P&gt;&lt;P&gt;Cx : 18 pF&lt;/P&gt;&lt;P&gt;Cy : 18 pF&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using __pe_initialize_hardware() of mqx\source\bsp\twrk20d50m\bsp_cm.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It often do not start the oscillation.&lt;/P&gt;&lt;P&gt;What can I do ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 09:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531195#M16418</guid>
      <dc:creator>daido</dc:creator>
      <dc:date>2016-08-16T09:07:58Z</dc:date>
    </item>
    <item>
      <title>Re: often not start oscillation MK10DN128VLH5</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531196#M16419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX 4.2 doesn't support the MK10DN128VLH5 device so I assume you are cloning the twr-k20d50m bsp, is it correct??&lt;/P&gt;&lt;P&gt;If you are using the same clock configuration then you don't need to modify the bsp_cm.c file, however if you need made some modification then you need to follow the attached document, this &lt;SPAN lang="EN-US"&gt;document that explains how to change the default clock configurations.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 20:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531196#M16419</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-08-16T20:53:28Z</dc:date>
    </item>
    <item>
      <title>Re: often not start oscillation MK10DN128VLH5</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531197#M16420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The oscillator curcuit of PK20DX128VFM5 in TWR-KM34Z50M is different from TWR-K20D50M's.&lt;/P&gt;&lt;P&gt;Is there any reason?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Minoru&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Aug 2016 05:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531197#M16420</guid>
      <dc:creator>daido</dc:creator>
      <dc:date>2016-08-17T05:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: often not start oscillation MK10DN128VLH5</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531198#M16421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Minoru,&lt;/P&gt;&lt;P&gt;CSTCE8M00G55-R0 Reference manual / datasheet says, that the resonator, has a built in loading capacitance 33pF&lt;/P&gt;&lt;P&gt;&lt;A href="http://pdf1.alldatasheet.com/datasheet-pdf/view/505165/MURATA/CSTCE8M00G55-R0.html" title="http://pdf1.alldatasheet.com/datasheet-pdf/view/505165/MURATA/CSTCE8M00G55-R0.html"&gt;CSTCE8M00G55-R0 pdf, CSTCE8M00G55-R0 description, CSTCE8M00G55-R0 datasheets, CSTCE8M00G55-R0 view ::: ALLDATASHEET :::&lt;/A&gt; &lt;/P&gt;&lt;P&gt;- Additional capacitive loading of the circuit may cause issues!&lt;/P&gt;&lt;P&gt;Moreover, if I am not mistaken the MCU supports the internal loading capacitors, they can be enabled in the SW.&lt;/P&gt;&lt;P&gt;And I guess, that there is also internal resistor inside the MCU&lt;/P&gt;&lt;P&gt;Please try to remove/depopulate the CAPs from the board.&lt;/P&gt;&lt;P&gt;And if the oscillator circuit is still unstable, check the SW settings as well. Oscillator High Gain mode (HGO=1) and the proper frequency range has to be selected in SW.&lt;/P&gt;&lt;P&gt;- I am the author of the TWR-KM34Z50M. I have copied the resonator components from other design. This resonator doesn't have internal loading caps, and the external capacitor values have been calculated for this resonator.&lt;/P&gt;&lt;P&gt;The main advantage was that the resonator component is available in small packages. - comparing to the crystals.&lt;/P&gt;&lt;P&gt;resonators are ususaly cheaper than precise crystals.&lt;/P&gt;&lt;P&gt;Anyway, there are disadvantages of the resonators:&lt;/P&gt;&lt;P&gt;1. (frequency deviation) The generated frequency is not so precise comparing to the crystals.&lt;/P&gt;&lt;P&gt;2. The frequency may vary from one component to other and with the enviromental influences.&lt;/P&gt;&lt;P&gt;- So for the precise timing, I would never use resonators again. And I would preffer crystal or canned osc.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michael G.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Aug 2016 07:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531198#M16421</guid>
      <dc:creator>michael_galda</dc:creator>
      <dc:date>2016-08-17T07:44:00Z</dc:date>
    </item>
    <item>
      <title>Re: often not start oscillation MK10DN128VLH5</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531199#M16422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I removed caps.&lt;/P&gt;&lt;P&gt;Although never oscillated, I increase caps using OSC0_CR register.&lt;/P&gt;&lt;P&gt;12pF stable&lt;/P&gt;&lt;P&gt;14pF stable&lt;/P&gt;&lt;P&gt;16pF stable&lt;/P&gt;&lt;P&gt;18pF stable&lt;/P&gt;&lt;P&gt;20pF stable&lt;/P&gt;&lt;P&gt;22pF unstable&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It might depend on the load caps...&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Minoru&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Aug 2016 10:39:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531199#M16422</guid>
      <dc:creator>daido</dc:creator>
      <dc:date>2016-08-17T10:39:37Z</dc:date>
    </item>
    <item>
      <title>Re: often not start oscillation MK10DN128VLH5</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531200#M16423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It depends if the external ones + their stray parasitic capacitance are not &amp;gt; 20pF due external component tolerances.&lt;/P&gt;&lt;P&gt;Standard cheap caps are +/- 20% tolerance in precision.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Aug 2016 11:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531200#M16423</guid>
      <dc:creator>michael_galda</dc:creator>
      <dc:date>2016-08-17T11:59:53Z</dc:date>
    </item>
    <item>
      <title>Re: often not start oscillation MK10DN128VLH5</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531201#M16424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A ceramic resonator with internal load caps does not require any external load caps. It just needs a feedback resistor. Do not add any internal capacitance in the MCU since the load caps are sufficient for oscillation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Aug 2016 14:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/often-not-start-oscillation-MK10DN128VLH5/m-p/531201#M16424</guid>
      <dc:creator>john_suchyta</dc:creator>
      <dc:date>2016-08-18T14:37:24Z</dc:date>
    </item>
  </channel>
</rss>