<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IP forwarding when running a web server in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/IP-forwarding-when-running-a-web-server/m-p/527407#M16381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I just have a quick question regarding the _IP_forward variable in MQX. As default this is set to false, but in the http server example it's set to true. I just wanted to know what the reason for this is and what the effects are. The reason I'm asking is beacuse when we run a program to monitor SNMP it says that all our products that have embedded web servers are routers, since the snmp node ipForwarding returns 1. It's not a big problem by any means, but it can be a bit missleading for our customers if our products gets mistaken for routers by&amp;nbsp; some SNMP monitoring programs. But would there be any negative effects if we didn't set _IP_forward to true when using a https server?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Aug 2016 08:33:23 GMT</pubDate>
    <dc:creator>jesperevertsson</dc:creator>
    <dc:date>2016-08-15T08:33:23Z</dc:date>
    <item>
      <title>IP forwarding when running a web server</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/IP-forwarding-when-running-a-web-server/m-p/527407#M16381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I just have a quick question regarding the _IP_forward variable in MQX. As default this is set to false, but in the http server example it's set to true. I just wanted to know what the reason for this is and what the effects are. The reason I'm asking is beacuse when we run a program to monitor SNMP it says that all our products that have embedded web servers are routers, since the snmp node ipForwarding returns 1. It's not a big problem by any means, but it can be a bit missleading for our customers if our products gets mistaken for routers by&amp;nbsp; some SNMP monitoring programs. But would there be any negative effects if we didn't set _IP_forward to true when using a https server?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 08:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/IP-forwarding-when-running-a-web-server/m-p/527407#M16381</guid>
      <dc:creator>jesperevertsson</dc:creator>
      <dc:date>2016-08-15T08:33:23Z</dc:date>
    </item>
    <item>
      <title>Re: IP forwarding when running a web server</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/IP-forwarding-when-running-a-web-server/m-p/527408#M16382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jesper;&lt;/P&gt;&lt;P&gt;_IP_forward is set to true when you want RTCS to forward packets between multiple interfaces (act like a router between subnets). It only makes sense to enable this if there are multiple interfaces.&lt;/P&gt;&lt;P&gt;Craig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 20:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/IP-forwarding-when-running-a-web-server/m-p/527408#M16382</guid>
      <dc:creator>EAI</dc:creator>
      <dc:date>2016-08-15T20:21:56Z</dc:date>
    </item>
    <item>
      <title>Re: IP forwarding when running a web server</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/IP-forwarding-when-running-a-web-server/m-p/527409#M16383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just add to Craig's good comments, let me give an example here, let's say you have two NICs, one (NIC1) is at address 192.168.2.1/24, and the other (NIC2) is 192.168.3.1/24.&amp;nbsp; If forwarding is enabled, and a packet comes in on NIC1 with a "destination address" of 192.168.3.9, your divices will resend that packet out of the NIC2.&amp;nbsp; If forwarding is not enabled, this packet will be discarded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 05:32:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/IP-forwarding-when-running-a-web-server/m-p/527409#M16383</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2016-08-16T05:32:39Z</dc:date>
    </item>
  </channel>
</rss>