<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: 100M Ethernet Negotiation</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516435#M16347</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Turns out that the mqx/bsp project includes code/a driver to init/control a ksz8041 which does not include writing to the correct registers to only negotiate 100M for a different PHY...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 15:08:49 GMT</pubDate>
    <dc:creator>mattitoikka</dc:creator>
    <dc:date>2016-06-16T15:08:49Z</dc:date>
    <item>
      <title>100M Ethernet Negotiation</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516431#M16343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there anyway to initialize the ethernet/mac interface in MQX RTCS such that the PHY will force/advertise 100M only?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 18:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516431#M16343</guid>
      <dc:creator>mattitoikka</dc:creator>
      <dc:date>2016-06-07T18:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: 100M Ethernet Negotiation</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516432#M16344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Matti,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the Radek's answer in the next thread and let me know if this helps.&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.jiveon.com/thread/349680" title="https://freescale.jiveon.com/thread/349680"&gt;10Mbps with LAN8720 and K70 - Communication wit... | NXP Community&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 19:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516432#M16344</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-06-07T19:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: 100M Ethernet Negotiation</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516433#M16345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, but the thread you linked seems to discuss periodically checking link status/speed in order to re-initialize the enet module to support adapting to different speeds/duplex when the ethernet connection is unplugged and re-connected to different switches/hubs during runtime. It didn't really help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to set my PHY to only advertise 100M. It looks like changing “Auto-negotiation” to “Full_Duplex_100M” in the ENET_default_params struct in init_enet.c (for me it is located at mqx\source\bsp\myProject\init_enet.c, but may be different for others depending on how you setup a project) should solve my issue. However, I have made the change and my PHY still auto-negotiates...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any other ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Matti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 15:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516433#M16345</guid>
      <dc:creator>mattitoikka</dc:creator>
      <dc:date>2016-06-10T15:52:55Z</dc:date>
    </item>
    <item>
      <title>Re: 100M Ethernet Negotiation</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516434#M16346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;Hello Matti,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;Yes you are right, you need to &lt;/SPAN&gt;&lt;SPAN style="color: #303030;"&gt;change this setting in the ENET_default_params[] structure which is located in the file init_enet.c. In that structure change the second element from "Auto_Negotiate" to "Half_Duplex_10M" or "Full_Duplex_10M", "Half_Duplex_100M" or "Full_Duplex_100M".&amp;nbsp; After these changes you need to &lt;STRONG&gt;Rebuild&lt;/STRONG&gt; the &lt;STRONG&gt;BSP, PSP and RTCS&lt;/STRONG&gt; libraries.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-weight: normal; font-style: normal; font-size: 15px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f; text-align: left; text-indent: 0px;"&gt;&lt;/P&gt;&lt;P style="font-weight: normal; font-style: normal; font-size: 15px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f; text-align: left; text-indent: 0px;"&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59779i301380C6DC6604A4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 19:28:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516434#M16346</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-06-10T19:28:55Z</dc:date>
    </item>
    <item>
      <title>Re: 100M Ethernet Negotiation</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516435#M16347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Turns out that the mqx/bsp project includes code/a driver to init/control a ksz8041 which does not include writing to the correct registers to only negotiate 100M for a different PHY...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 15:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/100M-Ethernet-Negotiation/m-p/516435#M16347</guid>
      <dc:creator>mattitoikka</dc:creator>
      <dc:date>2016-06-16T15:08:49Z</dc:date>
    </item>
  </channel>
</rss>