<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 RTCS receive 802.3 problem - MQX 4.2</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-receive-802-3-problem-MQX-4-2/m-p/507019#M16221</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MQX 4.2. I need to receive an 802.3 frame.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have successfully called ENET_open(). I can successfully send the 802.3 frame using ENET_send_raw(). I have verified the frame is sent and is formatted correctly using Wireshark.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have looked at the thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/62463"&gt;Sending Ethernet 2 frames&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this thread a user said they had to set the following define to zero to receive an 802.3 frame. I have tried that with no success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define RTCSCFG_IP_DISABLE_DIRECTED_BROADCAST 0&amp;nbsp; //this did not help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Feb 2016 23:02:30 GMT</pubDate>
    <dc:creator>kfranz</dc:creator>
    <dc:date>2016-02-12T23:02:30Z</dc:date>
    <item>
      <title>RTCS receive 802.3 problem - MQX 4.2</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-receive-802-3-problem-MQX-4-2/m-p/507019#M16221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MQX 4.2. I need to receive an 802.3 frame.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have successfully called ENET_open(). I can successfully send the 802.3 frame using ENET_send_raw(). I have verified the frame is sent and is formatted correctly using Wireshark.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have looked at the thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/62463"&gt;Sending Ethernet 2 frames&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this thread a user said they had to set the following define to zero to receive an 802.3 frame. I have tried that with no success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define RTCSCFG_IP_DISABLE_DIRECTED_BROADCAST 0&amp;nbsp; //this did not help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 23:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-receive-802-3-problem-MQX-4-2/m-p/507019#M16221</guid>
      <dc:creator>kfranz</dc:creator>
      <dc:date>2016-02-12T23:02:30Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS receive 802.3 problem - MQX 4.2</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-receive-802-3-problem-MQX-4-2/m-p/507020#M16222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In case it matters, we are using a K64.&lt;/P&gt;&lt;P&gt;For more information read about the following registers in the K64:&lt;/P&gt;&lt;P&gt;ENET_RCR bits PROM (promiscuous) and BC_REJ (broadcast), and ENET_GAUR, ENET_GALR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The solution is after the open, call ENET_join().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// destination MAC address&lt;/P&gt;&lt;P&gt;void fnOpen802_3(void) {&lt;/P&gt;&lt;P&gt;unsigned char aucDestMac[6] = {0x01,0x02,0x03,0x00,0x00,0x00};&lt;/P&gt;&lt;P&gt;ip_mreq&amp;nbsp;&amp;nbsp;&amp;nbsp; mreq;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if ((ENET_open(&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RTCS_get_enet_handle(ipcfg_get_ihandle(BSP_DEFAULT_ENET_DEVICE))),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x5566, // EtherType, ethernet type&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnMy802_3_Receive,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RTCS_get_enet_handle(ipcfg_get_ihandle(BSP_DEFAULT_ENET_DEVICE)))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; )) != ENET_OK)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //error&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ENET_join((RTCS_get_enet_handle(ipcfg_get_ihandle(BSP_DEFAULT_ENET_DEVICE))),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x5566, // EtherType, ethernet type&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; aucDestMac);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Feb 2016 15:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-receive-802-3-problem-MQX-4-2/m-p/507020#M16222</guid>
      <dc:creator>kfranz</dc:creator>
      <dc:date>2016-02-16T15:06:24Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS receive 802.3 problem - MQX 4.2</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-receive-802-3-problem-MQX-4-2/m-p/507021#M16223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kfranz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, MQX does not provide support for low layer data handling. The functions that you are using are RTCS internal, as you may see they are not documented. It may be possible to get inside the BSP to implement this use case, but I am not aware of all the implications that this process may have. Meaningful manipulation to the BSP is necessary to achieve this task, and this kind of support is only provided by our professional services team. You can contact them at &lt;A href="https://community.nxp.com/www.nxp.com/services" target="test_blank"&gt;www.nxp.com/services&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand you can use ENET baremetal code. In the KQRUG you can find an example.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf" title="http://cache.nxp.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf"&gt;http://www.nxp.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Feb 2016 23:40:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-receive-802-3-problem-MQX-4-2/m-p/507021#M16223</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2016-02-16T23:40:53Z</dc:date>
    </item>
  </channel>
</rss>