<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: My MQX4.2 projects often get stuck in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/My-MQX4-2-projects-often-get-stuck/m-p/493061#M16031</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yufei:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you need to check whether MQX rtos is running. Did you call OSA_Start in your application?&lt;/P&gt;&lt;P&gt;You can debug the task with MQX TAD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you the latest KSDK1.3, you can refer to the MQX rtos i2c example in the installation path&lt;/P&gt;&lt;P&gt;C:\Freescale\KSDK_1.3.0\examples\frdmk64f\demo_apps\i2c_rtos\i2c_rtos_mqx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Dec 2015 07:30:20 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2015-12-21T07:30:20Z</dc:date>
    <item>
      <title>My MQX4.2 projects often get stuck</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/My-MQX4-2-projects-often-get-stuck/m-p/493060#M16030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone, my program is run on the MQX4.2 KSDK1.2 based board is frdmk64f&lt;/P&gt;&lt;P&gt;But my program on MQX4.2 always met with some strange questions&lt;/P&gt;&lt;P&gt;For example, the same code, such as I2C or CAN communication transmit and receive code,&lt;/P&gt;&lt;P&gt;the same code which was run ok in a project without MQX RTOS &lt;/P&gt;&lt;P&gt;when it&amp;nbsp; was run on the project with MQX will be have some strange problems&lt;/P&gt;&lt;P&gt;For example, when I put the code of&amp;nbsp; CAN initialization and CAN transmission&amp;nbsp; together in a function,it will run ok,but when I Separate them in two function then run in a task,it will not to be sent.&lt;/P&gt;&lt;P&gt;I2C exactly the same code works ok in a project without MQX rtos, but will be sent out in the waveform is not right with the&amp;nbsp; MQX rtos .&lt;/P&gt;&lt;P&gt;and the project with mqx often when I Modify some parameters&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm really more dizzy,&lt;/P&gt;&lt;P&gt;Even I was only create One MQX task in the project it was&amp;nbsp; still have&amp;nbsp; the problem!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Dec 2015 04:36:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/My-MQX4-2-projects-often-get-stuck/m-p/493060#M16030</guid>
      <dc:creator>wyflsxy</dc:creator>
      <dc:date>2015-12-18T04:36:53Z</dc:date>
    </item>
    <item>
      <title>Re: My MQX4.2 projects often get stuck</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/My-MQX4-2-projects-often-get-stuck/m-p/493061#M16031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yufei:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you need to check whether MQX rtos is running. Did you call OSA_Start in your application?&lt;/P&gt;&lt;P&gt;You can debug the task with MQX TAD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you the latest KSDK1.3, you can refer to the MQX rtos i2c example in the installation path&lt;/P&gt;&lt;P&gt;C:\Freescale\KSDK_1.3.0\examples\frdmk64f\demo_apps\i2c_rtos\i2c_rtos_mqx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Dec 2015 07:30:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/My-MQX4-2-projects-often-get-stuck/m-p/493061#M16031</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2015-12-21T07:30:20Z</dc:date>
    </item>
  </channel>
</rss>