<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Working sets (MQX-specific) in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Working-sets-MQX-specific/m-p/489629#M15949</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, both assumptions are correct.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Dec 2015 17:08:47 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2015-12-28T17:08:47Z</dc:date>
    <item>
      <title>Working sets (MQX-specific)</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Working-sets-MQX-specific/m-p/489628#M15948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm making a new MQX BSP for a K10.&amp;nbsp; One thing I'm a little confused on is the directory structure.&amp;nbsp; I had previously used the twr-k20d50m board and had MQX running on it.&amp;nbsp; If I import the working set for one of the examples for the twr-k20d50m, I see the BSP, PSP, and application trees.&amp;nbsp; If I look at the properties for the directories and files within them, I see directories for the peripheral drivers such as:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/bsp_twrk20d50m/Peripheral_IO_Drivers/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see that same directory in:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_2\mqx\build\kds\bsp_twrk20d50m&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the contents of Peripheral_IO_Drivers is empty in that exact location.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It appears that the contents are actually being referenced in:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_2\mqx\source&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Interestingly, KDS seems to show that they are actually in the bsp build directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, am I correct that it's actually referencing directories in the MQX source directory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That leads to my next question, my new BSP is based on the K60.&amp;nbsp; The BSP porting tool made a new one alright, but it includes build directories for ethernet and USB, which don't apply to the K10.&amp;nbsp; I'm assuming that these can be removed from the project to ignore them (I've already excluded them in the build) without affecting the contents of the MQX source directory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2015 16:26:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Working-sets-MQX-specific/m-p/489628#M15948</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2015-12-16T16:26:43Z</dc:date>
    </item>
    <item>
      <title>Re: Working sets (MQX-specific)</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Working-sets-MQX-specific/m-p/489629#M15949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, both assumptions are correct.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 17:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Working-sets-MQX-specific/m-p/489629#M15949</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-12-28T17:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: Working sets (MQX-specific)</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Working-sets-MQX-specific/m-p/489630#M15950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 15:12:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Working-sets-MQX-specific/m-p/489630#M15950</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2016-01-04T15:12:24Z</dc:date>
    </item>
  </channel>
</rss>