<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: USB CDC virtual com example program on TWR70</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-virtual-com-example-program-on-TWR70/m-p/482464#M15829</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sue,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which example are you using? I was able to run cdc_vcom_twrk70f120m example that is located at: &amp;lt;MQX_4_2_PATH&amp;gt;/\usb\device\examples\cdc\virtual_com\build\cw10gcc and it worked well when ddrdata debug configuration was used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac Avila&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Feb 2016 22:45:11 GMT</pubDate>
    <dc:creator>isaacavila</dc:creator>
    <dc:date>2016-02-29T22:45:11Z</dc:date>
    <item>
      <title>USB CDC virtual com example program on TWR70</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-virtual-com-example-program-on-TWR70/m-p/482463#M15828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having problems running this example when I build the example for ddrdata.&lt;/P&gt;&lt;P&gt;If I build for sramdata then the USB enumerates correctly and I can run the example in windows 7&lt;/P&gt;&lt;P&gt;If I build the same program for ddrdata then the USB doesn't enumerate and windows 7 gives an error that the device is unknown.&lt;/P&gt;&lt;P&gt;I get numerous USB_APP_BUS_RESET events but never get the USB_APP_ENUM_COMPLETE event.&lt;/P&gt;&lt;P&gt;I've checked the linker files and the .usb_bdt is set in the sram data and aligned corectly in both linker files - the only difference between the two is the start address&lt;/P&gt;&lt;P&gt;Am running out of things to look for.&lt;/P&gt;&lt;P&gt;Any ideas would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2016 16:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-virtual-com-example-program-on-TWR70/m-p/482463#M15828</guid>
      <dc:creator>sueneal</dc:creator>
      <dc:date>2016-02-23T16:45:36Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC virtual com example program on TWR70</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-virtual-com-example-program-on-TWR70/m-p/482464#M15829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sue,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which example are you using? I was able to run cdc_vcom_twrk70f120m example that is located at: &amp;lt;MQX_4_2_PATH&amp;gt;/\usb\device\examples\cdc\virtual_com\build\cw10gcc and it worked well when ddrdata debug configuration was used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac Avila&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Feb 2016 22:45:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-virtual-com-example-program-on-TWR70/m-p/482464#M15829</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2016-02-29T22:45:11Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC virtual com example program on TWR70</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-virtual-com-example-program-on-TWR70/m-p/482465#M15830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Isaac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was using the kds build  - I managed to get it working as I realised that my bsp had BSPCFG_HAS_SRAM_POOL and  MQX_USE_UNCACHED_MEM turned off Once I turned them on it worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sue&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Mar 2016 08:52:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-virtual-com-example-program-on-TWR70/m-p/482465#M15830</guid>
      <dc:creator>sueneal</dc:creator>
      <dc:date>2016-03-01T08:52:20Z</dc:date>
    </item>
  </channel>
</rss>