<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with bootloader_vybrid on Vybrid DS-5 Win7 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475884#M15671</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;Hi Alejandro,&lt;BR /&gt; I will try different version of DS-5 at weekend. I have tried only different MQX4.1_Vybrid. With that it behaves same way. Same version of DS-5 just for Linux with MQX4.2 it is working just fine.&lt;BR /&gt; I think it is problem with debugger or file that it uses for its settings probably from MQX4.2. I can transfer my compiled code to SD card and run it. When I use Baremetal project I am able to debug it, transfer it to SD card and run it. Yesterday I was working with that Baremetal project and it works fine but when I ran this project today it is behave same way as other projects. I have few Eclipse based IDE's. I am using these IDE's each for different type of project. Is it possible that this could be the cause? Could they affects its settings for projects or for them selfs somehow?&lt;BR /&gt; I am attaching warnings and errors from different example project with MQX4.2, DS-5 v5.23.1 win7:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt; &lt;BR /&gt; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33687iED4A38A59B1B38BD/image-size/large?v=v2&amp;amp;px=999" title="Warnings.jpg" alt="Warnings.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33622i97EC106E7CB7C44A/image-size/large?v=v2&amp;amp;px=999" title="ErrorDebuger.jpg" alt="ErrorDebuger.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt; I do not know if it is related but I have also problem with cloning MQX4.2 library. I have tried that on two PCs both with win7. I have compiled MQX4.1 without problems. Details are in thread below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;&lt;A href="https://community.nxp.com/thread/383336"&gt;Cloning Wizard MQX4.2 Vybrid error&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jan 2016 09:55:18 GMT</pubDate>
    <dc:creator>cerma</dc:creator>
    <dc:date>2016-01-15T09:55:18Z</dc:date>
    <item>
      <title>Problem with bootloader_vybrid on Vybrid DS-5 Win7</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475882#M15669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;Hello,&lt;BR /&gt; I am using win 7 64bit with MQX4.2 and DS-5 5.23.1(32bit). I am able to build project and it is working when I upload *.bin files to SD card (MQX on A5 and Baremetal project on M4). But I am unable to debug bootloader from your examples (&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;bootloader_vybrid)&lt;/SPAN&gt; on A5 there is always error (picture attached). I can debug both applications for A5 and M4 core but not bootloader.&lt;BR /&gt; I have tried same bootloader example under Linux (Ubuntu 14.04 LTS 32bit, MQX RTOS 4.2.0 and linux version of DS-5 5.23.1). On Linux version of DS5 is no problem to debug bootloader and it is fully functional. Do you have any idea why is it not working on windows?&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53993iD74168D2A258274B/image-size/large?v=v2&amp;amp;px=999" title="DS5.jpg" alt="DS5.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jan 2016 09:25:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475882#M15669</guid>
      <dc:creator>cerma</dc:creator>
      <dc:date>2016-01-08T09:25:11Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with bootloader_vybrid on Vybrid DS-5 Win7</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475883#M15670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me try to find the reason of the problem.&lt;/P&gt;&lt;P&gt;Have you tried with a different DS-5 version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 16:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475883#M15670</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2016-01-14T16:17:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with bootloader_vybrid on Vybrid DS-5 Win7</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475884#M15671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;Hi Alejandro,&lt;BR /&gt; I will try different version of DS-5 at weekend. I have tried only different MQX4.1_Vybrid. With that it behaves same way. Same version of DS-5 just for Linux with MQX4.2 it is working just fine.&lt;BR /&gt; I think it is problem with debugger or file that it uses for its settings probably from MQX4.2. I can transfer my compiled code to SD card and run it. When I use Baremetal project I am able to debug it, transfer it to SD card and run it. Yesterday I was working with that Baremetal project and it works fine but when I ran this project today it is behave same way as other projects. I have few Eclipse based IDE's. I am using these IDE's each for different type of project. Is it possible that this could be the cause? Could they affects its settings for projects or for them selfs somehow?&lt;BR /&gt; I am attaching warnings and errors from different example project with MQX4.2, DS-5 v5.23.1 win7:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt; &lt;BR /&gt; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33687iED4A38A59B1B38BD/image-size/large?v=v2&amp;amp;px=999" title="Warnings.jpg" alt="Warnings.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33622i97EC106E7CB7C44A/image-size/large?v=v2&amp;amp;px=999" title="ErrorDebuger.jpg" alt="ErrorDebuger.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt; I do not know if it is related but I have also problem with cloning MQX4.2 library. I have tried that on two PCs both with win7. I have compiled MQX4.1 without problems. Details are in thread below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;&lt;A href="https://community.nxp.com/thread/383336"&gt;Cloning Wizard MQX4.2 Vybrid error&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 09:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475884#M15671</guid>
      <dc:creator>cerma</dc:creator>
      <dc:date>2016-01-15T09:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with bootloader_vybrid on Vybrid DS-5 Win7</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475885#M15672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have tried one more thing. I have ran new project with dual_core_ds5_m4 example. This project occasionally run in debuger correctly. I have tried various combinations of HW interconnection (different USB port, shorter cabel, unplug USB before every run,...). I still don't have clue what could go wrong. Below is attached output for both cases:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36270i03C78F4FB2368607/image-size/large?v=v2&amp;amp;px=999" title="test1.jpg" alt="test1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36272i95CC748BF3CBFD8A/image-size/large?v=v2&amp;amp;px=999" title="test2.jpg" alt="test2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 12:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475885#M15672</guid>
      <dc:creator>cerma</dc:creator>
      <dc:date>2016-01-15T12:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with bootloader_vybrid on Vybrid DS-5 Win7</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475886#M15673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;I have ran project on different PC with Win7 32bit and with installation MQX4_2 and DS-5 v5.23.1. Project behaves same way as in previous cases. I am attaching my project, which gives me error when I run it in debug mode. Do you can run it on Tower at your office? Do you can check if project settings is ok? I am attaching user_config as well. With PSP and BSP would be zip too big.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 12:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475886#M15673</guid>
      <dc:creator>cerma</dc:creator>
      <dc:date>2016-01-18T12:10:04Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with bootloader_vybrid on Vybrid DS-5 Win7</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475887#M15674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;I have tested my project with older version of DS-5 5.22. It behaves same way. When I import same project to Linux and its version of DS-5 and I just change all necessarily paths I am able to debug it without problems. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: black;"&gt;I have no idea what to do next.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 08:24:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-with-bootloader-vybrid-on-Vybrid-DS-5-Win7/m-p/475887#M15674</guid>
      <dc:creator>cerma</dc:creator>
      <dc:date>2016-01-19T08:24:22Z</dc:date>
    </item>
  </channel>
</rss>