<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 why I can't use the MFS in different task?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/why-I-can-t-use-the-MFS-in-different-task/m-p/472056#M15620</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try to use the MQX MFS to save file in task_a,and the SD card and MFS are init in task_b, when the program goes to error_code = ioctl(filesystem_handle, IO_IOCTL_CREATE_SUBDIR,(uint32_t *)file_path); the program will stop, what is the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'am using my own borad and the MQX 4.1, both are tested to be ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Dec 2015 13:43:47 GMT</pubDate>
    <dc:creator>botaoyang</dc:creator>
    <dc:date>2015-12-09T13:43:47Z</dc:date>
    <item>
      <title>why I can't use the MFS in different task?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/why-I-can-t-use-the-MFS-in-different-task/m-p/472056#M15620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try to use the MQX MFS to save file in task_a,and the SD card and MFS are init in task_b, when the program goes to error_code = ioctl(filesystem_handle, IO_IOCTL_CREATE_SUBDIR,(uint32_t *)file_path); the program will stop, what is the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'am using my own borad and the MQX 4.1, both are tested to be ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 13:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/why-I-can-t-use-the-MFS-in-different-task/m-p/472056#M15620</guid>
      <dc:creator>botaoyang</dc:creator>
      <dc:date>2015-12-09T13:43:47Z</dc:date>
    </item>
    <item>
      <title>Re: why I can't use the MFS in different task?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/why-I-can-t-use-the-MFS-in-different-task/m-p/472057#M15621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; think the two tasks have different context, I don't see your code but I suggest you check the input parameters, filesystem_handle, is it a valid pointer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 06:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/why-I-can-t-use-the-MFS-in-different-task/m-p/472057#M15621</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2015-12-28T06:03:08Z</dc:date>
    </item>
  </channel>
</rss>