<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MQX code for K65 TSI  in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-code-for-K65-TSI/m-p/466248#M15544</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is not an example using the K65 device, however you can use the below application note (and software) as reference.&lt;/P&gt;&lt;P&gt;This appnote shows examples using:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Segment LCD&lt;/LI&gt;&lt;LI&gt;Real-time Clock&lt;/LI&gt;&lt;LI&gt;FlexMemory&lt;/LI&gt;&lt;LI&gt;SPI interface to Wi-Fi system&lt;/LI&gt;&lt;LI&gt; FlexBus external bus interface to graphic LCD display&lt;/LI&gt;&lt;LI&gt;ADC connection to touch screen overlay&lt;/LI&gt;&lt;LI&gt;I2C communication with external Freescale sensors&lt;/LI&gt;&lt;LI&gt;Ethernet Controller&lt;/LI&gt;&lt;LI&gt;Hardware Touch Sensor Interface (TSI)&lt;/LI&gt;&lt;LI&gt;Low power modes with Low-leakage Wakeup Unit (LLWU)&lt;/LI&gt;&lt;LI&gt;General-purpose input/output (GPIO)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCA…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346_SW.exe" title="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346_SW.exe"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346_SW.exe&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Feb 2016 17:17:49 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2016-02-18T17:17:49Z</dc:date>
    <item>
      <title>MQX code for K65 TSI</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-code-for-K65-TSI/m-p/466247#M15543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any example project for using TSI module and its interrupt in MQX? I tried porting KSDK code for TSI onto MQX and I am getting confused whether I am doing it properly or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be helpful if anyone can share any working project or at least guide me to get a working code in MQX for TSI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2016 13:48:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-code-for-K65-TSI/m-p/466247#M15543</guid>
      <dc:creator>annamol</dc:creator>
      <dc:date>2016-02-17T13:48:43Z</dc:date>
    </item>
    <item>
      <title>Re: MQX code for K65 TSI</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-code-for-K65-TSI/m-p/466248#M15544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is not an example using the K65 device, however you can use the below application note (and software) as reference.&lt;/P&gt;&lt;P&gt;This appnote shows examples using:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Segment LCD&lt;/LI&gt;&lt;LI&gt;Real-time Clock&lt;/LI&gt;&lt;LI&gt;FlexMemory&lt;/LI&gt;&lt;LI&gt;SPI interface to Wi-Fi system&lt;/LI&gt;&lt;LI&gt; FlexBus external bus interface to graphic LCD display&lt;/LI&gt;&lt;LI&gt;ADC connection to touch screen overlay&lt;/LI&gt;&lt;LI&gt;I2C communication with external Freescale sensors&lt;/LI&gt;&lt;LI&gt;Ethernet Controller&lt;/LI&gt;&lt;LI&gt;Hardware Touch Sensor Interface (TSI)&lt;/LI&gt;&lt;LI&gt;Low power modes with Low-leakage Wakeup Unit (LLWU)&lt;/LI&gt;&lt;LI&gt;General-purpose input/output (GPIO)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCA…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346_SW.exe" title="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346_SW.exe"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4346_SW.exe&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 17:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-code-for-K65-TSI/m-p/466248#M15544</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-02-18T17:17:49Z</dc:date>
    </item>
  </channel>
</rss>