<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CONFIGURING RTC ALARM AS LLWU SOURCE K65 - MQX in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/CONFIGURING-RTC-ALARM-AS-LLWU-SOURCE-K65-MQX/m-p/460699#M15472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX integrates a Low-Power Management (LPM) driver to take advantage of the low-power operating modes in MQX applications.&lt;/P&gt;&lt;P&gt;Please check the below application note:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4447.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4447.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4447.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I would recommend running the LPM example located at [mqx_dir]\mqx\examples\lowpower on a supported Kinetis tower board. It shows using the RTC to wakeup out of various low power modes, including the LPM_OPERATION_MODE_STOP that you are interested in. The clocks are restored after wake-up to enable the UART to output the results. This is done in the LPM driver, in the file [mqx_dir]\mqx\source\io\lpm\lpm_kinetis.c&lt;/P&gt;&lt;P&gt;Also note that you cannot go into LLS mode while using the debugger, so the register readings after waking up will have to be done via a UART printf.&lt;/P&gt;&lt;P&gt;I hope this helps, have a great day,&lt;BR /&gt; Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Mar 2016 21:07:34 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2016-03-29T21:07:34Z</dc:date>
    <item>
      <title>CONFIGURING RTC ALARM AS LLWU SOURCE K65 - MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CONFIGURING-RTC-ALARM-AS-LLWU-SOURCE-K65-MQX/m-p/460698#M15471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to configure RTC alarm as wakeup source for K65F180M processor. The following changes were made in bsp and application for the same.&lt;/P&gt;&lt;P&gt;In init_lpm.c,&lt;/P&gt;&lt;P&gt;// LPM_OPERATION_MODE_STOP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPM_CPU_POWER_MODE_LLS,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Index of predefined mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Additional mode flags&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_PE1_WUPE3(1),&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Mode wake up events from pins 0..3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Mode wake up events from pins 4..7&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Mode wake up events from pins 8..11&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_PE4_WUPE13(1),&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Mode wake up events from pins 12..15&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;STRONG&gt;&amp;nbsp; LLWU_ME_WUME5_MASK &lt;/STRONG&gt;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_ME_WUME0_MASK Mode wake up events from internal input sources -&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; },&lt;/P&gt;&lt;P&gt;as RTC alarm is mapped onto LLWU_ME5.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the core is not coming out of LLS mode. RTC alarm works fine independently and transition between power modes VLPR and LLS also works fine.&amp;nbsp; I want the core to out of LLS mode when RTC interrupt occurs at the predefined period.&amp;nbsp; I am attaching the MQX code written for the same. Please do help me with the configuration, as i believe I am missing something in configuration. The development environment is IAR and a K65 eval kit.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Do we need to use RTC wakeup pin?&lt;/LI&gt;&lt;LI&gt;Is it because RTC clock gets disabled in LLS?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I have attached the code being used. One more doubt, is it possible to use debugger in low power modes like LLS, VLLSx. The bare metal implementation of power down modes allows debugger to be used even in low power modes. Is it possible in mqx? If yes, how can we do that&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338735"&gt;main.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 11:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CONFIGURING-RTC-ALARM-AS-LLWU-SOURCE-K65-MQX/m-p/460698#M15471</guid>
      <dc:creator>annamol</dc:creator>
      <dc:date>2016-03-08T11:03:06Z</dc:date>
    </item>
    <item>
      <title>Re: CONFIGURING RTC ALARM AS LLWU SOURCE K65 - MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CONFIGURING-RTC-ALARM-AS-LLWU-SOURCE-K65-MQX/m-p/460699#M15472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX integrates a Low-Power Management (LPM) driver to take advantage of the low-power operating modes in MQX applications.&lt;/P&gt;&lt;P&gt;Please check the below application note:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4447.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4447.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4447.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I would recommend running the LPM example located at [mqx_dir]\mqx\examples\lowpower on a supported Kinetis tower board. It shows using the RTC to wakeup out of various low power modes, including the LPM_OPERATION_MODE_STOP that you are interested in. The clocks are restored after wake-up to enable the UART to output the results. This is done in the LPM driver, in the file [mqx_dir]\mqx\source\io\lpm\lpm_kinetis.c&lt;/P&gt;&lt;P&gt;Also note that you cannot go into LLS mode while using the debugger, so the register readings after waking up will have to be done via a UART printf.&lt;/P&gt;&lt;P&gt;I hope this helps, have a great day,&lt;BR /&gt; Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Mar 2016 21:07:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CONFIGURING-RTC-ALARM-AS-LLWU-SOURCE-K65-MQX/m-p/460699#M15472</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-03-29T21:07:34Z</dc:date>
    </item>
    <item>
      <title>Re: CONFIGURING RTC ALARM AS LLWU SOURCE K65 - MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CONFIGURING-RTC-ALARM-AS-LLWU-SOURCE-K65-MQX/m-p/460700#M15473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The core was not waking up because of a silly mistake i did in code. I forgot to enable interrupt for and had registered call back alone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Enable RTC interrupt&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _bsp_int_init(INT_RTC , 2 , 0 , TRUE);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // enable interrupt&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _bsp_int_enable(INT_RTC);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyways thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Jun 2016 09:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CONFIGURING-RTC-ALARM-AS-LLWU-SOURCE-K65-MQX/m-p/460700#M15473</guid>
      <dc:creator>annamol</dc:creator>
      <dc:date>2016-06-04T09:23:18Z</dc:date>
    </item>
  </channel>
</rss>