<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RAW ethernet frames in MQX 4.1 in TWR-K70F120M in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/RAW-ethernet-frames-in-MQX-4-1-in-TWR-K70F120M/m-p/458060#M15399</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to obtain level-2 Ethernet frame, beginning with MAC source/destination fields, etc (according to &lt;A href="https://en.wikipedia.org/wiki/Ethernet_frame"&gt;https://en.wikipedia.org/wiki/Ethernet_frame&lt;/A&gt;). For longer time, I'm browsing MQC code, especially files such us &lt;EM&gt;macnet_receive.c&lt;/EM&gt; and &lt;EM&gt;enrecv.c&lt;/EM&gt;. Like stated in other post &lt;A _jive_internal="true" href="https://community.nxp.com/thread/350082"&gt;https://community.freescale.com/thread/350082&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've started with interrupt function &lt;STRONG&gt;void MACNET_RX_ISR (void&amp;nbsp;&amp;nbsp;&amp;nbsp; *enet)&lt;/STRONG&gt; which deals with &lt;STRONG&gt;ENET_CONTEXT_STRUCT_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp; enet_ptr&lt;EM&gt;. &lt;/EM&gt;&lt;/STRONG&gt;This pointer is later processed in &lt;STRONG style="color: #303030;"&gt;MACNET_process_rx_bds(ENET_CONTEXT_STRUCT_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp; enet_ptr)&lt;/STRONG&gt; function, where inside there is introduced &lt;STRONG&gt;buffer &lt;/STRONG&gt;where both are being passed to &lt;STRONG&gt;ENET_find_receiver(ENET_CONTEXT_STRUCT_PTR&amp;nbsp; enet_ptr, ENET_HEADER_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; packet_ptr, uint32_t *length_ptr). &lt;/STRONG&gt;I've 3-rd party code that requires just a pointer to Ethernet frame. Should I pass then a &lt;STRONG&gt;buffer&lt;EM&gt; &lt;/EM&gt;&lt;/STRONG&gt;or &lt;STRONG&gt;&lt;SPAN style="color: #303030;"&gt;ENET_CONTEXT_STRUCT_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp; enet_ptr&lt;/SPAN&gt;&lt;EM style="color: #303030;"&gt; &lt;/EM&gt;&lt;/STRONG&gt;&lt;SPAN style="color: #303030;"&gt;? Thank you for help. I couldn't find any info about this 2-layer in documentation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;Maciej&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Sep 2015 11:46:58 GMT</pubDate>
    <dc:creator>maciejwdowiarz-</dc:creator>
    <dc:date>2015-09-17T11:46:58Z</dc:date>
    <item>
      <title>RAW ethernet frames in MQX 4.1 in TWR-K70F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RAW-ethernet-frames-in-MQX-4-1-in-TWR-K70F120M/m-p/458060#M15399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to obtain level-2 Ethernet frame, beginning with MAC source/destination fields, etc (according to &lt;A href="https://en.wikipedia.org/wiki/Ethernet_frame"&gt;https://en.wikipedia.org/wiki/Ethernet_frame&lt;/A&gt;). For longer time, I'm browsing MQC code, especially files such us &lt;EM&gt;macnet_receive.c&lt;/EM&gt; and &lt;EM&gt;enrecv.c&lt;/EM&gt;. Like stated in other post &lt;A _jive_internal="true" href="https://community.nxp.com/thread/350082"&gt;https://community.freescale.com/thread/350082&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've started with interrupt function &lt;STRONG&gt;void MACNET_RX_ISR (void&amp;nbsp;&amp;nbsp;&amp;nbsp; *enet)&lt;/STRONG&gt; which deals with &lt;STRONG&gt;ENET_CONTEXT_STRUCT_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp; enet_ptr&lt;EM&gt;. &lt;/EM&gt;&lt;/STRONG&gt;This pointer is later processed in &lt;STRONG style="color: #303030;"&gt;MACNET_process_rx_bds(ENET_CONTEXT_STRUCT_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp; enet_ptr)&lt;/STRONG&gt; function, where inside there is introduced &lt;STRONG&gt;buffer &lt;/STRONG&gt;where both are being passed to &lt;STRONG&gt;ENET_find_receiver(ENET_CONTEXT_STRUCT_PTR&amp;nbsp; enet_ptr, ENET_HEADER_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; packet_ptr, uint32_t *length_ptr). &lt;/STRONG&gt;I've 3-rd party code that requires just a pointer to Ethernet frame. Should I pass then a &lt;STRONG&gt;buffer&lt;EM&gt; &lt;/EM&gt;&lt;/STRONG&gt;or &lt;STRONG&gt;&lt;SPAN style="color: #303030;"&gt;ENET_CONTEXT_STRUCT_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp; enet_ptr&lt;/SPAN&gt;&lt;EM style="color: #303030;"&gt; &lt;/EM&gt;&lt;/STRONG&gt;&lt;SPAN style="color: #303030;"&gt;? Thank you for help. I couldn't find any info about this 2-layer in documentation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;Maciej&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 11:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RAW-ethernet-frames-in-MQX-4-1-in-TWR-K70F120M/m-p/458060#M15399</guid>
      <dc:creator>maciejwdowiarz-</dc:creator>
      <dc:date>2015-09-17T11:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: RAW ethernet frames in MQX 4.1 in TWR-K70F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RAW-ethernet-frames-in-MQX-4-1-in-TWR-K70F120M/m-p/458061#M15400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Maciej, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For MQX 4.1 only ENET driver and RTCS Ethernet media layer has VLAN-specific definition that has influence on Ethernet frame size.&lt;/P&gt;&lt;P&gt;It allocates additional 4 byte of space for IEEE802.1Q tag in Ethernet frame. But there is no VLAN-specific code in RTCS stack.&lt;/P&gt;&lt;P&gt;Please check the new MQX release (4.2).&lt;/P&gt;&lt;P&gt;You can find below the new feactures implemented in this release:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RTCS TCP/IPv4 and TCP/IPv6(optional) stacks - version 4.2.0 (same as in KSDK 1.2.0)&lt;/P&gt;&lt;P&gt;• The new TLSF best-fit memory allocators were added.&lt;/P&gt;&lt;P&gt;• LLMNR - RTCS newly support Link-Local Multicast Name Resolution (LLMNR) Server. This protocol allows resolving simple label names on local subnet without the necessity of having a DNS server.&lt;/P&gt;&lt;P&gt;• Added DHCP Client v6 client application protocol support (Available in MQX RTOS IPv6 Add-on for purchase).&lt;/P&gt;&lt;P&gt;• Added Telnet Client IPv6 protocol support; API of this component was changed (Available in MQX RTOS IPv6 Add-on for purchase).&lt;/P&gt;&lt;P&gt;• Added TFTP Client/Server IPv6 protocol support; API of this component was changed (Available in MQX IPv6 Add-on for purchase).&lt;/P&gt;&lt;P&gt;• Added support of WebSocket server as part of Http server code. The implementation was fully tested by AutoBahn test suite.&lt;/P&gt;&lt;P&gt;• HTTP server was extended by SSL support (Available in WolfSSL add-on for evaluation).&lt;/P&gt;&lt;P&gt;• Socket code has been updated by various BSD compatible options and flags.&lt;/P&gt;&lt;P&gt;• ARP cache handling was modified to protect RTCS against DoS Attack.&lt;/P&gt;&lt;P&gt;• For more details see complete change log in the &amp;lt;MQX&amp;gt;/rtcs/rtcs_changelog.txt file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 21:22:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RAW-ethernet-frames-in-MQX-4-1-in-TWR-K70F120M/m-p/458061#M15400</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-09-23T21:22:52Z</dc:date>
    </item>
    <item>
      <title>Re: RAW ethernet frames in MQX 4.1 in TWR-K70F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RAW-ethernet-frames-in-MQX-4-1-in-TWR-K70F120M/m-p/458062#M15401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried to use code from function VNIC_FEC_Init(). That is, initializing device and registering to protocol. However, no frames are calling the callback. Could you help me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Code below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;void Callback&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; (&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PCB_PTR&amp;nbsp; pcb,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* [IN] the received packet */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; void&amp;nbsp;&amp;nbsp;&amp;nbsp; *handle&amp;nbsp;&amp;nbsp;&amp;nbsp; /* [IN] the IP interface structure */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; )&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("\nreceived enet 0x0800 frame\n");&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PCB_free(pcb);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void Ethernet_task (uint32_t initial_data)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _enet_address&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; enet_address;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; IPCFG_IP_ADDRESS_DATA&amp;nbsp;&amp;nbsp;&amp;nbsp; ip_data;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; error;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _enet_handle enet_ptr;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ip_data.ip = ENET_IPADDR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ip_data.mask = ENET_IPMASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ip_data.gateway = ENET_IPGATEWAY;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ENET_get_mac_address (BSP_DEFAULT_ENET_DEVICE, ENET_IPADDR, enet_address);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; error = ENET_initialize (BSP_DEFAULT_ENET_DEVICE, enet_address, 0, &amp;amp;enet_ptr);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; if(error != ENET_OK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("ENET_Initialization Failed\n");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _task_block();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("START Ethernet task\n");&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (ENET_open(enet_ptr, 0x0800, Callback, ipcfg_get_ihandle(BSP_DEFAULT_ENET_DEVICE)) != ENET_OK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Registering an EtherType value for IPv4 protocol failed.\n");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _task_block();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("ETHER TASK FINISHED\n");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 11:19:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RAW-ethernet-frames-in-MQX-4-1-in-TWR-K70F120M/m-p/458062#M15401</guid>
      <dc:creator>maciejwdowiarz-</dc:creator>
      <dc:date>2015-10-05T11:19:43Z</dc:date>
    </item>
  </channel>
</rss>