<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is the difference when starting with the debugger instead of reset in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456889#M15343</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, and the interrupts work correctly but I think I found the problem. The interrupts seem to be only in RAM so after a reset the beginning of the flash is "empty". It seems like that with the debugger a different start address is used and that confused me :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jul 2015 10:02:08 GMT</pubDate>
    <dc:creator>simonteki</dc:creator>
    <dc:date>2015-07-08T10:02:08Z</dc:date>
    <item>
      <title>What is the difference when starting with the debugger instead of reset</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456886#M15340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with KDS 3.0.0 with the TWR-K60F120M and my project works if I use the gdb debugger. But as soon as I have an reset the SW get stuck in an undefined area (No source available for "0xfffffffe" ) and the reset light on the board is half lit. Can the use of the interrupt vectors in RAM cause such problems? As the reset vector isn't handled correctly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2015 10:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456886#M15340</guid>
      <dc:creator>simonteki</dc:creator>
      <dc:date>2015-07-07T10:31:04Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference when starting with the debugger instead of reset</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456887#M15341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, it is definitely a problem with the interrupts in RAM. Even if I use the PE generated code for it, it fails after a reset. Any ideas what I am missing? Shouldn't' it jump to address 0 and start up normally? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 08:12:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456887#M15341</guid>
      <dc:creator>simonteki</dc:creator>
      <dc:date>2015-07-08T08:12:18Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference when starting with the debugger instead of reset</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456888#M15342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did you ever perform vector relocation in your application?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 09:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456888#M15342</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-07-08T09:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference when starting with the debugger instead of reset</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456889#M15343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, and the interrupts work correctly but I think I found the problem. The interrupts seem to be only in RAM so after a reset the beginning of the flash is "empty". It seems like that with the debugger a different start address is used and that confused me :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 10:02:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/What-is-the-difference-when-starting-with-the-debugger-instead/m-p/456889#M15343</guid>
      <dc:creator>simonteki</dc:creator>
      <dc:date>2015-07-08T10:02:08Z</dc:date>
    </item>
  </channel>
</rss>