<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: How do I disable the MQX FlexCAN driver?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-do-I-disable-the-MQX-FlexCAN-driver/m-p/455863#M15315</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excellent. I've been calling the init(), so I'll just stop calling it. This will make it a lot easier to swap between the two without having to rebuild as much. Thanks a bunch!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Aug 2015 14:06:03 GMT</pubDate>
    <dc:creator>robertyork</dc:creator>
    <dc:date>2015-08-21T14:06:03Z</dc:date>
    <item>
      <title>How do I disable the MQX FlexCAN driver?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-do-I-disable-the-MQX-FlexCAN-driver/m-p/455861#M15313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been struggling with the MQX 4.1 FlexCAN driver. So far, I've gotten through most of the issues, but I'm getting stuck on receiving data. Rather than bang my head trying to figure it out, It's been suggested I try the PE CAN driver. I've been told it's a lot simpler.&amp;nbsp; One note I saw was that I need to disable the MQX FlexCAN driver in the user_config.h. However, I can't find any mention of any CAN driver in user_config.h. I had to modify the init_gpio.c file to point to the correct pins for my board, but I don't see anything else about disabling it. Any idea how I stop MQX from initializing it? The only other method I could think of would be to remove the configuration info from init_gpio.c&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 15:34:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-do-I-disable-the-MQX-FlexCAN-driver/m-p/455861#M15313</guid>
      <dc:creator>robertyork</dc:creator>
      <dc:date>2015-08-20T15:34:57Z</dc:date>
    </item>
    <item>
      <title>Re: How do I disable the MQX FlexCAN driver?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-do-I-disable-the-MQX-FlexCAN-driver/m-p/455862#M15314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Robert,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default the driver is disable. Some of the device drivers such as Timer, FlexCAN, RTC, etc. and the interrupt controller drivers implement a custom API and do not follow the standard driver interface. That means,the FlexCAN driver is not POSIX, only POSIX standard I/O are defined in the user_config.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to able the driver you need to use the function flexcan_init ().&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 23:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-do-I-disable-the-MQX-FlexCAN-driver/m-p/455862#M15314</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-08-20T23:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: How do I disable the MQX FlexCAN driver?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-do-I-disable-the-MQX-FlexCAN-driver/m-p/455863#M15315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excellent. I've been calling the init(), so I'll just stop calling it. This will make it a lot easier to swap between the two without having to rebuild as much. Thanks a bunch!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 14:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-do-I-disable-the-MQX-FlexCAN-driver/m-p/455863#M15315</guid>
      <dc:creator>robertyork</dc:creator>
      <dc:date>2015-08-21T14:06:03Z</dc:date>
    </item>
  </channel>
</rss>