<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: _Bool type</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Bool-type/m-p/452777#M15194</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yvan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below link,&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/321128"&gt;MQX 4.1 bool type conflict issues&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Let me know if this helps, &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2015 19:19:17 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2015-07-28T19:19:17Z</dc:date>
    <item>
      <title>_Bool type</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Bool-type/m-p/452776#M15193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What kind of variable is &lt;STRONG&gt;_Bool&lt;/STRONG&gt; ?&lt;/P&gt;&lt;P&gt;I must replace it by &lt;STRONG&gt;uint32_t&lt;/STRONG&gt; in &lt;STRONG&gt;C:\Freescale\CW MCU v10.6\MCU\ARM_GCC_Support\ewl\EWL_C\include\stdbool.h&lt;/STRONG&gt; because with the use of Atheros AR4100, the boolean definition must be :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* NOTE: A_BOOL is a type that is used in various WMI commands and events.&lt;/P&gt;&lt;P&gt; * as such it is a type that is shared between the wifi chipset and the host.&lt;/P&gt;&lt;P&gt; * It is required for that reason that A_BOOL be treated as a 32-bit/4-byte type.*/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, is it possible to have now a conflict&amp;nbsp; (CW 10.6 + MQX 4.2) ? With CW 10.5 + MQX 4.1.1, there were no problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 10:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Bool-type/m-p/452776#M15193</guid>
      <dc:creator>yb</dc:creator>
      <dc:date>2015-07-28T10:56:04Z</dc:date>
    </item>
    <item>
      <title>Re: _Bool type</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Bool-type/m-p/452777#M15194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yvan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below link,&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/321128"&gt;MQX 4.1 bool type conflict issues&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Let me know if this helps, &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 19:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Bool-type/m-p/452777#M15194</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-07-28T19:19:17Z</dc:date>
    </item>
  </channel>
</rss>