<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Console output</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Console-output/m-p/447834#M15000</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to run some of the MQX 4.2 demos.&amp;nbsp; I have finally got the hello2 demo with a twrk70f120 to compile and download to my tower board.&amp;nbsp; It appears to run, but I do not get any of the messages.&amp;nbsp; I am assuming that these show up in the console window, but I only see the compiler messages.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where should these messages appear?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Jul 2015 15:17:26 GMT</pubDate>
    <dc:creator>dporada</dc:creator>
    <dc:date>2015-07-01T15:17:26Z</dc:date>
    <item>
      <title>Console output</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Console-output/m-p/447834#M15000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to run some of the MQX 4.2 demos.&amp;nbsp; I have finally got the hello2 demo with a twrk70f120 to compile and download to my tower board.&amp;nbsp; It appears to run, but I do not get any of the messages.&amp;nbsp; I am assuming that these show up in the console window, but I only see the compiler messages.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where should these messages appear?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 15:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Console-output/m-p/447834#M15000</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2015-07-01T15:17:26Z</dc:date>
    </item>
    <item>
      <title>Re: Console output</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Console-output/m-p/447835#M15001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Donald,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the video attached&lt;/P&gt;&lt;P&gt;The default console configured in MQX for the TWR-K70F120M is OSJTAG - USB mini connector.&lt;/P&gt;&lt;P&gt;Serial I/O is a channel routed via combined OSBDM/OSJTAG debugging and communication port directly to the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Default Serial I/O Channel Settings:&lt;/P&gt;&lt;P&gt;• Baud Rate 115200&lt;/P&gt;&lt;P&gt;• Data bits 8&lt;/P&gt;&lt;P&gt;• No parity&lt;/P&gt;&lt;P&gt;• 1 stop bit and no flow control&lt;/P&gt;&lt;P&gt;Pre-defined default I/O channel setting is specified for each board in the mqx\source\bsp\&amp;lt;board_name&amp;gt;&lt;/P&gt;&lt;P&gt;\board_name.h header file. This setting can be overridden in the user_config.h file by adding this code and rebuilding the&lt;/P&gt;&lt;P&gt;BSP library.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 17:46:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Console-output/m-p/447835#M15001</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-07-01T17:46:43Z</dc:date>
    </item>
  </channel>
</rss>