<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to stop FlexCan &amp;quot;CAN_RX_MSG_BUFFER_OVERRUN&amp;quot;, message rate to high, how to select just one message every 100ms in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-stop-FlexCan-quot-CAN-RX-MSG-BUFFER-OVERRUN-quot-message/m-p/444441#M14876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an API "flexcan_set_bitrate" in FSL FlexCAN driver,&amp;nbsp; not sure whether it is what you are looking for.&lt;/P&gt;&lt;P&gt;Can you specify you detail settings of each node?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Nov 2015 07:52:27 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2015-11-04T07:52:27Z</dc:date>
    <item>
      <title>How to stop FlexCan "CAN_RX_MSG_BUFFER_OVERRUN", message rate to high, how to select just one message every 100ms</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-stop-FlexCan-quot-CAN-RX-MSG-BUFFER-OVERRUN-quot-message/m-p/444440#M14875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using a k20dx256 with the FlexCan controllers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The test code works fine from MQX between two of our boards, when I attach a third node and try to read the messages I get an error, CAN_RX_MSG_BUFFER_OVERRUN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In looking at the sending node I can see it is dumping messages on the bus at about 1k/sec. The first message is received correctly and then all others get the overrun error. I think the data is invalid in the mailbox because of the overrun error. It does not change and should be changing.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I don't have control over the sender of the messages, so I would like to read messages at the rate of 10/sec instead of 1000/sec. But I am not sure how to do this or the best practice. Should I turn off interrupts and is there then a polling mechanism, or should I disable and re-enable the interrupts based on a timer for a single message. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to learn the basics of FlexCan so any help would be very welcome.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 07:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-stop-FlexCan-quot-CAN-RX-MSG-BUFFER-OVERRUN-quot-message/m-p/444440#M14875</guid>
      <dc:creator>Cdn_aye</dc:creator>
      <dc:date>2015-10-30T07:05:19Z</dc:date>
    </item>
    <item>
      <title>Re: How to stop FlexCan "CAN_RX_MSG_BUFFER_OVERRUN", message rate to high, how to select just one message every 100ms</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-stop-FlexCan-quot-CAN-RX-MSG-BUFFER-OVERRUN-quot-message/m-p/444441#M14876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an API "flexcan_set_bitrate" in FSL FlexCAN driver,&amp;nbsp; not sure whether it is what you are looking for.&lt;/P&gt;&lt;P&gt;Can you specify you detail settings of each node?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Nov 2015 07:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-stop-FlexCan-quot-CAN-RX-MSG-BUFFER-OVERRUN-quot-message/m-p/444441#M14876</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2015-11-04T07:52:27Z</dc:date>
    </item>
  </channel>
</rss>