<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SCI High speed in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164196#M1478</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oscar,&lt;/P&gt;&lt;P&gt;It's been awhile since I ran a test to see how fast the UART can run on ColdFire but what I recall is that the raw UART signal was fine but the UART transceiver has a lower max frequency capability.&amp;nbsp; I think I used oscope on input and output of transceiver to see the signal integrity to determine what was the system max frequency/baud I could use.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2011 20:24:21 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2011-09-02T20:24:21Z</dc:date>
    <item>
      <title>SCI High speed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164193#M1475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to communicate at serial high speed (460800 bps and 921600 bps) but I received wrong characters.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My design:&lt;/P&gt;&lt;P&gt;- I'm using the serial MQX driver (3.7) in interrupt mode and I configured it&amp;nbsp;for this speed (other speeds works well).&amp;nbsp;&lt;/P&gt;&lt;P&gt;- I'm using a 48MHz crystal. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I read that it's possible to use&amp;nbsp;(the baudrate register supports it).&lt;/P&gt;&lt;P&gt;Any idea about this topic?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 14:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164193#M1475</guid>
      <dc:creator>oscar</dc:creator>
      <dc:date>2011-09-02T14:04:21Z</dc:date>
    </item>
    <item>
      <title>Re: SCI High speed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164194#M1476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Oscar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have had same issues with MQX 3.7 with TWRK60 BSP . Follow this link for the details and a possible solution :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="87446" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/87446" jivemacro="thread" title="https://community.freescale.com/thread/87446"&gt;https://community.freescale.com/thread/87446&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 14:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164194#M1476</guid>
      <dc:creator>GottiLuca</dc:creator>
      <dc:date>2011-09-02T14:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: SCI High speed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164195#M1477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First, thanks for your quick response.&lt;/P&gt;&lt;P&gt;I saw your suggestion but&amp;nbsp;I'm using the &amp;nbsp;MCF52259 and it doesn't has a Baud Rate Fine Adjust (BRFA) register or similar....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 14:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164195#M1477</guid>
      <dc:creator>oscar</dc:creator>
      <dc:date>2011-09-02T14:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: SCI High speed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164196#M1478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oscar,&lt;/P&gt;&lt;P&gt;It's been awhile since I ran a test to see how fast the UART can run on ColdFire but what I recall is that the raw UART signal was fine but the UART transceiver has a lower max frequency capability.&amp;nbsp; I think I used oscope on input and output of transceiver to see the signal integrity to determine what was the system max frequency/baud I could use.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 20:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164196#M1478</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-09-02T20:24:21Z</dc:date>
    </item>
    <item>
      <title>Re: SCI High speed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164197#M1479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's a communication between 2 microcontrollers ( no transceivers used) . The problem is:&amp;nbsp;High %error&amp;nbsp;transmission&amp;nbsp;when when&amp;nbsp;using the internal clock source...I'm thinking to use a external clock source...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2011 19:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SCI-High-speed/m-p/164197#M1479</guid>
      <dc:creator>oscar</dc:creator>
      <dc:date>2011-09-06T19:04:35Z</dc:date>
    </item>
  </channel>
</rss>