<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックChanging where MQX_template_list is located</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Changing-where-MQX-template-list-is-located/m-p/431789#M14443</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to create my first MQX project from scratch. I am using the IAR Embedded Workbench so I went ahead and copied an existing project to a new folder and renamed it. I chose the gpio example since my procjet will use gpio. I managed to compile and run the project from the new location so everything is fine so far. Then I wanted to move the MQX_template_list from gpio.c to my own file called main.cpp. However, now when I try to compile I get an error saying "&lt;/P&gt;&lt;P&gt;Error[Li005]: no definition for "MQX_template_list" [referenced from mqx_init.o(bsp.a)] ". I assume that somewhere it' specified that the MQX_template_list should be located in gpio.c so I need to change that. I just don't know where to find it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Apr 2015 09:49:55 GMT</pubDate>
    <dc:creator>jesperevertsson</dc:creator>
    <dc:date>2015-04-22T09:49:55Z</dc:date>
    <item>
      <title>Changing where MQX_template_list is located</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Changing-where-MQX-template-list-is-located/m-p/431789#M14443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to create my first MQX project from scratch. I am using the IAR Embedded Workbench so I went ahead and copied an existing project to a new folder and renamed it. I chose the gpio example since my procjet will use gpio. I managed to compile and run the project from the new location so everything is fine so far. Then I wanted to move the MQX_template_list from gpio.c to my own file called main.cpp. However, now when I try to compile I get an error saying "&lt;/P&gt;&lt;P&gt;Error[Li005]: no definition for "MQX_template_list" [referenced from mqx_init.o(bsp.a)] ". I assume that somewhere it' specified that the MQX_template_list should be located in gpio.c so I need to change that. I just don't know where to find it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 09:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Changing-where-MQX-template-list-is-located/m-p/431789#M14443</guid>
      <dc:creator>jesperevertsson</dc:creator>
      <dc:date>2015-04-22T09:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: Changing where MQX_template_list is located</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Changing-where-MQX-template-list-is-located/m-p/431790#M14444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I managed to get it to work. Since my code was in C++ I had to add extern "C" and now it works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 14:01:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Changing-where-MQX-template-list-is-located/m-p/431790#M14444</guid>
      <dc:creator>jesperevertsson</dc:creator>
      <dc:date>2015-04-22T14:01:11Z</dc:date>
    </item>
  </channel>
</rss>