<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX not booting in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-not-booting/m-p/430451#M14400</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Essentially I followed this guide to building a framework MQX project: &lt;A _jive_internal="true" data-containerid="11347" data-containertype="14" data-content-finding="Community" data-objectid="103405" data-objecttype="102" href="https://community.nxp.com/docs/DOC-103405"&gt;How To: Create a New MQX RTOS for KSDK Project in KDS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something must be configured incorrectly in the linker or startup code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I load the same code from the pre-built example project (rtos hello world), it works fine.&amp;nbsp; If I try to build my own project from scratch by following these instructions (which I will need to do with a custom board) I run into this issue that appears to be the WDOG_EWM_IRQHandler being called and causing a DefaultISR interrup , even though if you look at the board files the DISABLE_WDOG code appears to be set correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the stack trace which happens just a few ms after startup:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120298iBB1EBF7324ADA7D8/image-size/large?v=v2&amp;amp;px=999" title="21599_21599.png" alt="21599_21599.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49206i9E8900AA043F65EF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried creating an explicit handler for this (which doesn't fire), I don't know what else to do.&amp;nbsp; I'm new to the quirks of MQX but I don't know how to make a project that is any simpler and it's already showing issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Appreciate any help you can give here, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2015 18:15:13 GMT</pubDate>
    <dc:creator>josephgundel</dc:creator>
    <dc:date>2015-04-21T18:15:13Z</dc:date>
    <item>
      <title>MQX not booting</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-not-booting/m-p/430451#M14400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Essentially I followed this guide to building a framework MQX project: &lt;A _jive_internal="true" data-containerid="11347" data-containertype="14" data-content-finding="Community" data-objectid="103405" data-objecttype="102" href="https://community.nxp.com/docs/DOC-103405"&gt;How To: Create a New MQX RTOS for KSDK Project in KDS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something must be configured incorrectly in the linker or startup code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I load the same code from the pre-built example project (rtos hello world), it works fine.&amp;nbsp; If I try to build my own project from scratch by following these instructions (which I will need to do with a custom board) I run into this issue that appears to be the WDOG_EWM_IRQHandler being called and causing a DefaultISR interrup , even though if you look at the board files the DISABLE_WDOG code appears to be set correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the stack trace which happens just a few ms after startup:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120298iBB1EBF7324ADA7D8/image-size/large?v=v2&amp;amp;px=999" title="21599_21599.png" alt="21599_21599.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49206i9E8900AA043F65EF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried creating an explicit handler for this (which doesn't fire), I don't know what else to do.&amp;nbsp; I'm new to the quirks of MQX but I don't know how to make a project that is any simpler and it's already showing issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Appreciate any help you can give here, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2015 18:15:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-not-booting/m-p/430451#M14400</guid>
      <dc:creator>josephgundel</dc:creator>
      <dc:date>2015-04-21T18:15:13Z</dc:date>
    </item>
    <item>
      <title>Re: MQX not booting</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-not-booting/m-p/430452#M14401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please look at my answer here:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/511192#511192"&gt;https://community.freescale.com/message/511192#511192&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2015 16:27:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-not-booting/m-p/430452#M14401</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-04-30T16:27:27Z</dc:date>
    </item>
  </channel>
</rss>