<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Copy from USB drive in MQX 4.1 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Copy-from-USB-drive-in-MQX-4-1/m-p/426846#M14253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the following thread&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/485645"&gt;Re: Copy a big file: Neither the shell command nor the custom code work&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jun 2015 11:23:26 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2015-06-26T11:23:26Z</dc:date>
    <item>
      <title>Copy from USB drive in MQX 4.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Copy-from-USB-drive-in-MQX-4-1/m-p/426845#M14252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm developing an MQX-based application on a K70 and I'm facing an issue: &lt;/P&gt;&lt;P&gt;I wrote a shell custom command to copy a directory from the USB drive to the NAND filesystem, including subdirectories and files, but sometimes, expecially when a large file is copied, the procedure ends and after that I can't see the content of the key anymore. However I see that the filesystem is still mounted (as "b:"). &lt;/P&gt;&lt;P&gt;To check if the problem is inside my function or something else I tried the copy of a large file with the shell command "copy" and I see the same result. While debugging I noticed that the code fails during a read.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody have some suggestions about this or experienced something similar?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 08:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Copy-from-USB-drive-in-MQX-4-1/m-p/426845#M14252</guid>
      <dc:creator>acremonini</dc:creator>
      <dc:date>2015-06-24T08:49:56Z</dc:date>
    </item>
    <item>
      <title>Re: Copy from USB drive in MQX 4.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Copy-from-USB-drive-in-MQX-4-1/m-p/426846#M14253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the following thread&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/485645"&gt;Re: Copy a big file: Neither the shell command nor the custom code work&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2015 11:23:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Copy-from-USB-drive-in-MQX-4-1/m-p/426846#M14253</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2015-06-26T11:23:26Z</dc:date>
    </item>
  </channel>
</rss>