<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PWM (FTM0_CHx) support in TWRK60 and MQX in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163672#M1411</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can&amp;nbsp; use the Processor Expert (PEx) to customize BSP (since MQX version 3.7) that you can use in your MQX aplication.&amp;nbsp; Into such BSP project, you can add PEx components you need, for examaple you can use TimerUnit_LDD component to provide PWM functionality.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There is already a example BSP project inside MQX 3.7 using Processor Expert for Kinetis TWR-K60 board insed MQX directory ...\Freescale MQX 3.7\mqx\build\cw10\bsp_twrk60n512_pe. ﻿&lt;BR /&gt;This project contains an example of PWM component.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Usage of this BSP in application code is demonstrated in pe_demo project in the demo directory: ...\Freescale MQX 3.7\demo\pe_demo.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;I recommend to use these projects as a start otherwise you would need to configure many settings if you like to start from an empty project.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Regarding second question - yes, PEx works also in the free limited CW version.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Petr Hradsky&lt;BR /&gt;Processor Expert Support Team&lt;BR /&gt;&lt;BR /&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Aug 2011 19:46:09 GMT</pubDate>
    <dc:creator>ProcessorExpert</dc:creator>
    <dc:date>2011-08-31T19:46:09Z</dc:date>
    <item>
      <title>PWM (FTM0_CHx) support in TWRK60 and MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163671#M1410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;need to generate PWM-output signals (25kHz, 1024 steps) with FTM0_CH0..3.&lt;/P&gt;&lt;P&gt;Is there any example code or support in MQX's BSP or PSP-library.&lt;/P&gt;&lt;P&gt;Does CW's Processor Expert has any PWM component for K60?&lt;/P&gt;&lt;P&gt;Should the PE work in free (code size limited) CW, version is 10.1?&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2011 12:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163671#M1410</guid>
      <dc:creator>MarkP_</dc:creator>
      <dc:date>2011-08-31T12:42:00Z</dc:date>
    </item>
    <item>
      <title>Re: PWM (FTM0_CHx) support in TWRK60 and MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163672#M1411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can&amp;nbsp; use the Processor Expert (PEx) to customize BSP (since MQX version 3.7) that you can use in your MQX aplication.&amp;nbsp; Into such BSP project, you can add PEx components you need, for examaple you can use TimerUnit_LDD component to provide PWM functionality.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There is already a example BSP project inside MQX 3.7 using Processor Expert for Kinetis TWR-K60 board insed MQX directory ...\Freescale MQX 3.7\mqx\build\cw10\bsp_twrk60n512_pe. ﻿&lt;BR /&gt;This project contains an example of PWM component.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Usage of this BSP in application code is demonstrated in pe_demo project in the demo directory: ...\Freescale MQX 3.7\demo\pe_demo.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;I recommend to use these projects as a start otherwise you would need to configure many settings if you like to start from an empty project.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Regarding second question - yes, PEx works also in the free limited CW version.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Petr Hradsky&lt;BR /&gt;Processor Expert Support Team&lt;BR /&gt;&lt;BR /&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2011 19:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163672#M1411</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2011-08-31T19:46:09Z</dc:date>
    </item>
    <item>
      <title>Re: PWM (FTM0_CHx) support in TWRK60 and MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163673#M1412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The FTM_init component will generate a PWM.&amp;nbsp; However, in user code you have to use:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;﻿﻿﻿﻿FTMx_CxV = (unit32_t)0xXXXXUL;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;to set the pulse width.&amp;nbsp; PE initializes the FTMx_CxV registers incorrectly before the FTMx_SC register.&amp;nbsp; I believe that this will be fixed in 10.2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Clark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2011 02:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163673#M1412</guid>
      <dc:creator>Clark</dc:creator>
      <dc:date>2011-09-01T02:32:31Z</dc:date>
    </item>
    <item>
      <title>Re: PWM (FTM0_CHx) support in TWRK60 and MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163674#M1413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Than you for feedback, we have fixed this problem for upcoming CodeWarrior for MCUs V10.2 release.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Petr Hradsky&lt;BR /&gt;Processor Expert Support and Servicepacks Team&lt;BR /&gt;&lt;BR /&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2011 16:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/PWM-FTM0-CHx-support-in-TWRK60-and-MQX/m-p/163674#M1413</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2011-09-26T16:33:18Z</dc:date>
    </item>
  </channel>
</rss>